Could IMX6SL boot from NAND?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could IMX6SL boot from NAND?

Jump to solution
1,818 Views
shaohang_cui
Contributor I

I didn't see NAND flash in IMX6SLRM Chapter 8 like IMX6ULRM; Also I didn't find pin mux for NAND in imx6sl-pinfunc.h. Does it mean IMX6SL can't boot from NAND?

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
1,779 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shaohang

you are right, i.IMX6SL can't boot from NAND.

There is no GPMI(NAND) module in i.MX6SL.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,780 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shaohang

you are right, i.IMX6SL can't boot from NAND.

There is no GPMI(NAND) module in i.MX6SL.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------