Hi all,
I have two SDRAMs on my customize board. The CS pins are IOMUXC_GPIO_EMC_29_SEMC_CS0 and IOMUXC_GPIO_B0_02_SEMC_CSX03, and the start address are 0x80000000 and 0x8C0000000, respectively.
I used semc_sdram example code to set both of them. And the SDRAMs can be read and written correctly.
Next step, the semc related registers were read out and recorded. So I filled out these values to dcd.c and comment out BOARD_InitSEMC(). However, the values read from the second SDRAM were wrong (the first SDRAM is okay). And I have localized the problem which comes from Mode setting in dcd.c. But the IPTXDAT of the second one is the same as the first one, so I cannot ffigure out the reason.
There is a question I need to make sure. Could I initialize two SDRAMs by dcd.c, or just one?
my dcd.c:
/*
* Copyright 2020 NXP
* All rights reserved.
*
* SPDX-License-Identifier: BSD-3-Clause
*/
/***********************************************************************************************************************
* This file was generated by the MCUXpresso Config Tools. Any manual edits made to this file
* will be overwritten if the respective MCUXpresso Config Tools is used to update this file.
**********************************************************************************************************************/
#include "dcd.h"
/* Component ID definition, used by tools. */
#ifndef FSL_COMPONENT_ID
#define FSL_COMPONENT_ID "platform.drivers.xip_board"
#endif
#if defined(XIP_BOOT_HEADER_ENABLE) && (XIP_BOOT_HEADER_ENABLE == 1)
#if defined(XIP_BOOT_HEADER_DCD_ENABLE) && (XIP_BOOT_HEADER_DCD_ENABLE == 1)
#if defined(__CC_ARM) || defined(__ARMCC_VERSION) || defined(__GNUC__)
__attribute__((section(".boot_hdr.dcd_data")))
#elif defined(__ICCARM__)
#pragma location = ".boot_hdr.dcd_data"
#endif
/* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
!!GlobalInfo
product: DCDx V2.0
processor: MIMXRT1062xxxxA
package_id: MIMXRT1062DVL6A
mcu_data: ksdk2_0
processor_version: 0.0.0
board: MIMXRT1060-EVK
output_format: c_array
* BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS **********/
/* COMMENTS BELOW ARE USED AS SETTINGS FOR DCD DATA */
const uint8_t dcd_data[] = {
/* HEADER */
/* Tag */
0xD2,
/* Image Length limit 1768bytes*/
//0x04, 0x10,
0x05, 0x4C,
/* Version */
0x41,
/* COMMANDS */
//set first sdram
/* group: 'Imported Commands' */
/* #1.1-113, command header bytes for merged 'Write - value' command */
0xCC, 0x03, 0x8C, 0x04, //904=113*8+4
/* #1.1, command: write_value, address: CCM_CCGR0, value: 0xFFFFFFFF, size: 4 */
0x40, 0x0F, 0xC0, 0x68, 0xFF, 0xFF, 0xFF, 0xFF,
/* #1.2, command: write_value, address: CCM_CCGR1, value: 0xFFFFFFFF, size: 4 */
0x40, 0x0F, 0xC0, 0x6C, 0xFF, 0xFF, 0xFF, 0xFF,
/* #1.3, command: write_value, address: CCM_CCGR2, value: 0xFFFFFFFF, size: 4 */
0x40, 0x0F, 0xC0, 0x70, 0xFF, 0xFF, 0xFF, 0xFF,
/* #1.4, command: write_value, address: CCM_CCGR3, value: 0xFFFFFFFF, size: 4 */
0x40, 0x0F, 0xC0, 0x74, 0xFF, 0xFF, 0xFF, 0xFF,
/* #1.5, command: write_value, address: CCM_CCGR4, value: 0xFFFFFFFF, size: 4 */
0x40, 0x0F, 0xC0, 0x78, 0xFF, 0xFF, 0xFF, 0xFF,
/* #1.6, command: write_value, address: CCM_CCGR5, value: 0xFFFFFFFF, size: 4 */
0x40, 0x0F, 0xC0, 0x7C, 0xFF, 0xFF, 0xFF, 0xFF,
/* #1.7, command: write_value, address: CCM_CCGR6, value: 0xFFFFFFFF, size: 4 */
0x40, 0x0F, 0xC0, 0x80, 0xFF, 0xFF, 0xFF, 0xFF,
/* #1.8, command: write_value, address: CCM_ANALOG_PLL_SYS, value: 0x2001, size: 4 */
0x40, 0x0D, 0x80, 0x30, 0x00, 0x00, 0x20, 0x01,
/* #1.9, command: write_value, address: CCM_ANALOG_PFD_528, value: 0x1D0000, size: 4 */
0x40, 0x0D, 0x81, 0x00, 0x00, 0x1D, 0x00, 0x00,
/* #1.10, command: write_value, address: CCM_CBCDR, value: 0x10D40, size: 4 */
0x40, 0x0F, 0xC0, 0x14, 0x00, 0x01, 0x0D, 0x40,
/* #1.11, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_00, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x14, 0x00, 0x00, 0x00, 0x00,
/* #1.12, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_01, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x18, 0x00, 0x00, 0x00, 0x00,
/* #1.13, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_02, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x1C, 0x00, 0x00, 0x00, 0x00,
/* #1.14, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_03, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x20, 0x00, 0x00, 0x00, 0x00,
/* #1.15, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_04, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x24, 0x00, 0x00, 0x00, 0x00,
/* #1.16, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_05, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x28, 0x00, 0x00, 0x00, 0x00,
/* #1.17, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_06, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x2C, 0x00, 0x00, 0x00, 0x00,
/* #1.18, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_07, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x30, 0x00, 0x00, 0x00, 0x00,
/* #1.19, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_08, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x34, 0x00, 0x00, 0x00, 0x00,
/* #1.20, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_09, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x38, 0x00, 0x00, 0x00, 0x00,
/* #1.21, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_10, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x3C, 0x00, 0x00, 0x00, 0x00,
/* #1.22, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_11, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x40, 0x00, 0x00, 0x00, 0x00,
/* #1.23, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_12, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x44, 0x00, 0x00, 0x00, 0x00,
/* #1.24, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_13, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x48, 0x00, 0x00, 0x00, 0x00,
/* #1.25, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_14, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x4C, 0x00, 0x00, 0x00, 0x00,
/* #1.26, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_15, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x50, 0x00, 0x00, 0x00, 0x00,
/* #1.27, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_16, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x54, 0x00, 0x00, 0x00, 0x00,
/* #1.28, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_17, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x58, 0x00, 0x00, 0x00, 0x00,
/* #1.29, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_18, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x5C, 0x00, 0x00, 0x00, 0x00,
/* #1.30, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_19, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x60, 0x00, 0x00, 0x00, 0x00,
/* #1.31, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_20, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x64, 0x00, 0x00, 0x00, 0x00,
/* #1.32, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_21, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x68, 0x00, 0x00, 0x00, 0x00,
/* #1.33, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_22, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x6C, 0x00, 0x00, 0x00, 0x00,
/* #1.34, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_23, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x70, 0x00, 0x00, 0x00, 0x00,
/* #1.35, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_24, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x74, 0x00, 0x00, 0x00, 0x00,
/* #1.36, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_25, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x78, 0x00, 0x00, 0x00, 0x00,
/* #1.37, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_26, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x7C, 0x00, 0x00, 0x00, 0x00,
/* #1.38, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_27, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x80, 0x00, 0x00, 0x00, 0x00,
/* #1.39, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_28, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x84, 0x00, 0x00, 0x00, 0x00,
/* #1.40, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_29, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x88, 0x00, 0x00, 0x00, 0x00,
/* #1.41, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_30, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x8C, 0x00, 0x00, 0x00, 0x00,
/* #1.42, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_31, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x90, 0x00, 0x00, 0x00, 0x00,
/* #1.43, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_32, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x94, 0x00, 0x00, 0x00, 0x00,
/* #1.44, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_33, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x98, 0x00, 0x00, 0x00, 0x00,
/* #1.45, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_34, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0x9C, 0x00, 0x00, 0x00, 0x00,
/* #1.46, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_35, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0xA0, 0x00, 0x00, 0x00, 0x00,
/* #1.47, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_36, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0xA4, 0x00, 0x00, 0x00, 0x00,
/* #1.48, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_37, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0xA8, 0x00, 0x00, 0x00, 0x00,
/* #1.49, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_38, value: 0x00, size: 4 */
0x40, 0x1F, 0x80, 0xAC, 0x00, 0x00, 0x00, 0x00,
/* #1.50, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_39, value: 0x10, size: 4 */
0x40, 0x1F, 0x80, 0xB0, 0x00, 0x00, 0x00, 0x10,
/* #1.51, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_00, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x04, 0x00, 0x01, 0x10, 0xF9,
/* #1.52, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_01, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x08, 0x00, 0x01, 0x10, 0xF9,
/* #1.53, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_02, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x0C, 0x00, 0x01, 0x10, 0xF9,
/* #1.54, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_03, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x10, 0x00, 0x01, 0x10, 0xF9,
/* #1.55, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_04, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x14, 0x00, 0x01, 0x10, 0xF9,
/* #1.56, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_05, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x18, 0x00, 0x01, 0x10, 0xF9,
/* #1.57, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_06, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x1C, 0x00, 0x01, 0x10, 0xF9,
/* #1.58, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_07, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x20, 0x00, 0x01, 0x10, 0xF9,
/* #1.59, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_08, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x24, 0x00, 0x01, 0x10, 0xF9,
/* #1.60, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_09, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x28, 0x00, 0x01, 0x10, 0xF9,
/* #1.61, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_10, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x2C, 0x00, 0x01, 0x10, 0xF9,
/* #1.62, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_11, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x30, 0x00, 0x01, 0x10, 0xF9,
/* #1.63, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_12, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x34, 0x00, 0x01, 0x10, 0xF9,
/* #1.64, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_13, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x38, 0x00, 0x01, 0x10, 0xF9,
/* #1.65, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_14, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x3C, 0x00, 0x01, 0x10, 0xF9,
/* #1.66, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_15, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x40, 0x00, 0x01, 0x10, 0xF9,
/* #1.67, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_16, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x44, 0x00, 0x01, 0x10, 0xF9,
/* #1.68, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_17, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x48, 0x00, 0x01, 0x10, 0xF9,
/* #1.69, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_18, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x4C, 0x00, 0x01, 0x10, 0xF9,
/* #1.70, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_19, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x50, 0x00, 0x01, 0x10, 0xF9,
/* #1.71, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_20, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x54, 0x00, 0x01, 0x10, 0xF9,
/* #1.72, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_21, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x58, 0x00, 0x01, 0x10, 0xF9,
/* #1.73, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_22, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x5C, 0x00, 0x01, 0x10, 0xF9,
/* #1.74, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_23, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x60, 0x00, 0x01, 0x10, 0xF9,
/* #1.75, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_24, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x64, 0x00, 0x01, 0x10, 0xF9,
/* #1.76, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_25, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x68, 0x00, 0x01, 0x10, 0xF9,
/* #1.77, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_26, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x6C, 0x00, 0x01, 0x10, 0xF9,
/* #1.78, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_27, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x70, 0x00, 0x01, 0x10, 0xF9,
/* #1.79, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_28, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x74, 0x00, 0x01, 0x10, 0xF9,
/* #1.80, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_29, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x78, 0x00, 0x01, 0x10, 0xF9,
/* #1.81, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_30, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x7C, 0x00, 0x01, 0x10, 0xF9,
/* #1.82, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_31, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x80, 0x00, 0x01, 0x10, 0xF9,
/* #1.83, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_32, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x84, 0x00, 0x01, 0x10, 0xF9,
/* #1.84, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_33, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x88, 0x00, 0x01, 0x10, 0xF9,
/* #1.85, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_34, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x8C, 0x00, 0x01, 0x10, 0xF9,
/* #1.86, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_35, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x90, 0x00, 0x01, 0x10, 0xF9,
/* #1.87, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_36, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x94, 0x00, 0x01, 0x10, 0xF9,
/* #1.88, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_37, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x98, 0x00, 0x01, 0x10, 0xF9,
/* #1.89, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_38, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0x9C, 0x00, 0x01, 0x10, 0xF9,
/* #1.90, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_39, value: 0x110F9, size: 4 */
0x40, 0x1F, 0x82, 0xA0, 0x00, 0x01, 0x10, 0xF9,
/* #1.91, command: write_value, address: SEMC_MCR, value: 0x10000004, size: 4 */
0x40, 0x2F, 0x00, 0x00, 0x10, 0x00, 0x00, 0x04,
/* #1.92, command: write_value, address: SEMC_BMCR0, value: 0x30524, size: 4 */
0x40, 0x2F, 0x00, 0x08, 0x00, 0x03, 0x05, 0x24,
/* #1.93, command: write_value, address: SEMC_BMCR1, value: 0x6030524, size: 4 */
0x40, 0x2F, 0x00, 0x0C, 0x06, 0x03, 0x05, 0x24,
/* #1.94, command: write_value, address: SEMC_BR0, value: 0x8000001B, size: 4 */
0x40, 0x2F, 0x00, 0x10, 0x80, 0x00, 0x00, 0x1B,
/* #1.95, command: write_value, address: SEMC_BR1, value: 0x8200001B, size: 4 */
0x40, 0x2F, 0x00, 0x14, 0x82, 0x00, 0x00, 0x1B,
/* #1.96, command: write_value, address: SEMC_BR2, value: 0x8400001B, size: 4 */
0x40, 0x2F, 0x00, 0x18, 0x84, 0x00, 0x00, 0x1B,
/* #1.97, command: write_value, address: SEMC_BR3, value: 0x8600001B, size: 4 */
0x40, 0x2F, 0x00, 0x1C, 0x8C, 0x00, 0x00, 0x1B,
/* #1.98, command: write_value, address: SEMC_BR4, value: 0x90000021, size: 4 */
0x40, 0x2F, 0x00, 0x20, 0x90, 0x00, 0x00, 0x21,
/* #1.99, command: write_value, address: SEMC_BR5, value: 0xA0000019, size: 4 */
0x40, 0x2F, 0x00, 0x24, 0xA0, 0x00, 0x00, 0x19,
/* #1.100, command: write_value, address: SEMC_BR6, value: 0xA8000017, size: 4 */
0x40, 0x2F, 0x00, 0x28, 0xA8, 0x00, 0x00, 0x17,
/* #1.101, command: write_value, address: SEMC_BR7, value: 0xA900001B, size: 4 */
0x40, 0x2F, 0x00, 0x2C, 0xA9, 0x00, 0x00, 0x1B,
/* #1.102, command: write_value, address: SEMC_BR8, value: 0x21, size: 4 */
0x40, 0x2F, 0x00, 0x30, 0x00, 0x00, 0x00, 0x21,
/* #1.103, command: write_value, address: SEMC_IOCR, value: 0x79A8, size: 4 */
0x40, 0x2F, 0x00, 0x04, 0x00, 0x00, 0x30, 0x00,
/* #1.104, command: write_value, address: SEMC_SDRAMCR0, value: 0xF31, size: 4 */
0x40, 0x2F, 0x00, 0x40, 0x00, 0x00, 0x0F, 0x31,
/* #1.105, command: write_value, address: SEMC_SDRAMCR1, value: 0x652922, size: 4 */
0x40, 0x2F, 0x00, 0x44, 0x00, 0x66, 0x4B, 0x22,
/* #1.106, command: write_value, address: SEMC_SDRAMCR2, value: 0x10920, size: 4 */
0x40, 0x2F, 0x00, 0x48, 0x00, 0x09, 0x09, 0x0B,
/* #1.107, command: write_value, address: SEMC_SDRAMCR3, value: 0x50210A08, size: 4 */
0x40, 0x2F, 0x00, 0x4C, 0x08, 0x07, 0x0A, 0x00,
/* #1.108, command: write_value, address: SEMC_DBICR0, value: 0x21, size: 4 */
0x40, 0x2F, 0x00, 0x80, 0x00, 0x00, 0x00, 0x21,
/* #1.109, command: write_value, address: SEMC_DBICR1, value: 0x888888, size: 4 */
0x40, 0x2F, 0x00, 0x84, 0x00, 0x88, 0x88, 0x88,
/* #1.110, command: write_value, address: SEMC_IPCR1, value: 0x02, size: 4 */
0x40, 0x2F, 0x00, 0x94, 0x00, 0x00, 0x00, 0x02,
/* #1.111, command: write_value, address: SEMC_IPCR2, value: 0x00, size: 4 */
0x40, 0x2F, 0x00, 0x98, 0x00, 0x00, 0x00, 0x00,
/* #1.112, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */
0x40, 0x2F, 0x00, 0x90, 0x80, 0x00, 0x00, 0x00,
/* #1.113, command: write_value, address: SEMC_IPCMD, value: 0xA55A000F, size: 4 */
0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0F,
/* #2, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
/* #3.1-2, command header bytes for merged 'Write - value' command */
0xCC, 0x00, 0x14, 0x04,
/* #3.1, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */
0x40, 0x2F, 0x00, 0x90, 0x80, 0x00, 0x00, 0x00,
/* #3.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */
0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,
/* #4, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
/* #5.1-2, command header bytes for merged 'Write - value' command */
0xCC, 0x00, 0x14, 0x04,
/* #5.1, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */
0x40, 0x2F, 0x00, 0x90, 0x80, 0x00, 0x00, 0x00,
/* #5.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */
0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,
/* #6, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
/* #7.1-3, command header bytes for merged 'Write - value' command */
0xCC, 0x00, 0x1C, 0x04,
/* #7.1, command: write_value, address: SEMC_IPTXDAT, value: 0x33, size: 4 */
0x40, 0x2F, 0x00, 0xA0, 0x00, 0x00, 0x00, 0x33,
/* #7.2, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */
0x40, 0x2F, 0x00, 0x90, 0x80, 0x00, 0x00, 0x00,
/* #7.3, command: write_value, address: SEMC_IPCMD, value: 0xA55A000A, size: 4 */
0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0A,
/* #8, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
/* #9, command: write_value, address: SEMC_SDRAMCR3, value: 0x50210A09, size: 4 */
0xCC, 0x00, 0x0C, 0x04, 0x40, 0x2F, 0x00, 0x4C, 0x08, 0x07, 0x0A, 0x01,
//1040bytes
//set second sdram
0xCC, 0x00, 0xBC, 0x04, //188=23*8+4
/* #1.91, command: write_value, address: SEMC_MCR, value: 0x10000004, size: 4 */
0x40, 0x2F, 0x00, 0x00, 0x10, 0x00, 0x00, 0x04,
/* #1.92, command: write_value, address: SEMC_BMCR0, value: 0x30524, size: 4 */
0x40, 0x2F, 0x00, 0x08, 0x00, 0x03, 0x05, 0x24,
/* #1.93, command: write_value, address: SEMC_BMCR1, value: 0x6030524, size: 4 */
0x40, 0x2F, 0x00, 0x0C, 0x06, 0x03, 0x05, 0x24,
/* #1.94, command: write_value, address: SEMC_BR0, value: 0x8000001B, size: 4 */
0x40, 0x2F, 0x00, 0x10, 0x80, 0x00, 0x00, 0x1B,
/* #1.95, command: write_value, address: SEMC_BR1, value: 0x8200001B, size: 4 */
0x40, 0x2F, 0x00, 0x14, 0x82, 0x00, 0x00, 0x1B,
/* #1.96, command: write_value, address: SEMC_BR2, value: 0x8400001B, size: 4 */
0x40, 0x2F, 0x00, 0x18, 0x84, 0x00, 0x00, 0x1B,
/* #1.97, command: write_value, address: SEMC_BR3, value: 0x8600001B, size: 4 */
0x40, 0x2F, 0x00, 0x1C, 0x8C, 0x00, 0x00, 0x1B,
/* #1.98, command: write_value, address: SEMC_BR4, value: 0x90000021, size: 4 */
0x40, 0x2F, 0x00, 0x20, 0x90, 0x00, 0x00, 0x21,
/* #1.99, command: write_value, address: SEMC_BR5, value: 0xA0000019, size: 4 */
0x40, 0x2F, 0x00, 0x24, 0xA0, 0x00, 0x00, 0x19,
/* #1.100, command: write_value, address: SEMC_BR6, value: 0xA8000017, size: 4 */
0x40, 0x2F, 0x00, 0x28, 0xA8, 0x00, 0x00, 0x17,
/* #1.101, command: write_value, address: SEMC_BR7, value: 0xA900001B, size: 4 */
0x40, 0x2F, 0x00, 0x2C, 0xA9, 0x00, 0x00, 0x1B,
/* #1.102, command: write_value, address: SEMC_BR8, value: 0x21, size: 4 */
0x40, 0x2F, 0x00, 0x30, 0x00, 0x00, 0x00, 0x21,
/* #1.103, command: write_value, address: SEMC_IOCR, value: 0x79A8, size: 4 */
0x40, 0x2F, 0x00, 0x04, 0x00, 0x00, 0x30, 0x00,
/* #1.104, command: write_value, address: SEMC_SDRAMCR0, value: 0xF31, size: 4 */
0x40, 0x2F, 0x00, 0x40, 0x00, 0x00, 0x0F, 0x31,
/* #1.105, command: write_value, address: SEMC_SDRAMCR1, value: 0x652922, size: 4 */
0x40, 0x2F, 0x00, 0x44, 0x00, 0x66, 0x4B, 0x22,
/* #1.106, command: write_value, address: SEMC_SDRAMCR2, value: 0x10920, size: 4 */
0x40, 0x2F, 0x00, 0x48, 0x00, 0x09, 0x09, 0x0B,
/* #1.107, command: write_value, address: SEMC_SDRAMCR3, value: 0x50210A08, size: 4 */
0x40, 0x2F, 0x00, 0x4C, 0x08, 0x07, 0x0A, 0x00,
/* #1.108, command: write_value, address: SEMC_DBICR0, value: 0x21, size: 4 */
0x40, 0x2F, 0x00, 0x80, 0x00, 0x00, 0x00, 0x21,
/* #1.109, command: write_value, address: SEMC_DBICR1, value: 0x888888, size: 4 */
0x40, 0x2F, 0x00, 0x84, 0x00, 0x88, 0x88, 0x88,
/* #1.110, command: write_value, address: SEMC_IPCR1, value: 0x02, size: 4 */
0x40, 0x2F, 0x00, 0x94, 0x00, 0x00, 0x00, 0x02,
/* #1.111, command: write_value, address: SEMC_IPCR2, value: 0x00, size: 4 */
0x40, 0x2F, 0x00, 0x98, 0x00, 0x00, 0x00, 0x00,
/* #1.112, command: write_value, address: SEMC_IPCR0, value: 0x8C000000, size: 4 */
0x40, 0x2F, 0x00, 0x90, 0x8C, 0x00, 0x00, 0x00,
/* #1.113, command: write_value, address: SEMC_IPCMD, value: 0xA55A000F, size: 4 */
0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0F,
/* #4, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
/* #5.1-2, command header bytes for merged 'Write - value' command */
0xCC, 0x00, 0x14, 0x04,
/* #5.1, command: write_value, address: SEMC_IPCR0, value: 0x8C000000, size: 4 */
0x40, 0x2F, 0x00, 0x90, 0x8C, 0x00, 0x00, 0x00,
/* #3.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */
0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,
/* #4, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
/* #5.1-2, command header bytes for merged 'Write - value' command */
0xCC, 0x00, 0x14, 0x04,
/* #5.1, command: write_value, address: SEMC_IPCR0, value: 0x8C000000, size: 4 */
0x40, 0x2F, 0x00, 0x90, 0x8C, 0x00, 0x00, 0x00,
/* #5.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */
0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,
/* #6, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
/* #7.1-3, command header bytes for merged 'Write - value' command */
0xCC, 0x00, 0x1C, 0x04,
/* #7.1, command: write_value, address: SEMC_IPTXDAT, value: 0x33, size: 4 */
0x40, 0x2F, 0x00, 0xA0, 0x00, 0x00, 0x00, 0x33,
/* #7.2, command: write_value, address: SEMC_IPCR0, value: 0x8C000000, size: 4 */
0x40, 0x2F, 0x00, 0x90, 0x8C, 0x00, 0x00, 0x00,
/* #7.3, command: write_value, address: SEMC_IPCMD, value: 0xA55A000A, size: 4 */
0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0A,
/* #8, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
/* #9, command: write_value, address: SEMC_SDRAMCR3, value: 0x50210A09, size: 4 */
0xCC, 0x00, 0x0C, 0x04, 0x40, 0x2F, 0x00, 0x4C, 0x08, 0x07, 0x0A, 0x01};
/* BE CAREFUL MODIFYING THIS SETTINGS - IT IS YAML SETTINGS FOR TOOLS */
//316 bytes
#else
const uint8_t dcd_data[] = {0x00};
#endif /* XIP_BOOT_HEADER_DCD_ENABLE */
#endif /* XIP_BOOT_HEADER_ENABLE */
Best regards,
Doris