Could I initialize two SDRAMs by dcd.c?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could I initialize two SDRAMs by dcd.c?

Jump to solution
2,921 Views
MCW
Contributor III

Hi all,

I have two SDRAMs on my customize board. The CS pins are IOMUXC_GPIO_EMC_29_SEMC_CS0 and IOMUXC_GPIO_B0_02_SEMC_CSX03, and the start address are 0x80000000 and 0x8C0000000, respectively.

I used semc_sdram example code to set both of them. And the SDRAMs can be read and written correctly.

Next step, the semc related registers were read out and recorded. So I filled out these values to dcd.c and comment out BOARD_InitSEMC(). However, the values read from the second SDRAM were wrong (the first SDRAM is okay).  And I have localized the problem which comes from Mode setting in dcd.c. But the  IPTXDAT of the second one is the same as the first one, so I cannot ffigure out the reason.

There is a question I need to make sure. Could I initialize two SDRAMs by dcd.c, or just one?

my dcd.c:

/*
 * Copyright 2020 NXP
 * All rights reserved.
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */

/***********************************************************************************************************************
 * This file was generated by the MCUXpresso Config Tools. Any manual edits made to this file
 * will be overwritten if the respective MCUXpresso Config Tools is used to update this file.
 **********************************************************************************************************************/

#include "dcd.h"

/* Component ID definition, used by tools. */
#ifndef FSL_COMPONENT_ID
#define FSL_COMPONENT_ID "platform.drivers.xip_board"
#endif

#if defined(XIP_BOOT_HEADER_ENABLE) && (XIP_BOOT_HEADER_ENABLE == 1)
#if defined(XIP_BOOT_HEADER_DCD_ENABLE) && (XIP_BOOT_HEADER_DCD_ENABLE == 1)
#if defined(__CC_ARM) || defined(__ARMCC_VERSION) || defined(__GNUC__)
__attribute__((section(".boot_hdr.dcd_data")))
#elif defined(__ICCARM__)
#pragma location = ".boot_hdr.dcd_data"
#endif

/* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
!!GlobalInfo
product: DCDx V2.0
processor: MIMXRT1062xxxxA
package_id: MIMXRT1062DVL6A
mcu_data: ksdk2_0
processor_version: 0.0.0
board: MIMXRT1060-EVK
output_format: c_array
 * BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS **********/
/* COMMENTS BELOW ARE USED AS SETTINGS FOR DCD DATA */
const uint8_t dcd_data[] = {
	/* HEADER */
	/* Tag */
	0xD2,
	/* Image Length limit 1768bytes*/ 
	//0x04, 0x10,
	0x05, 0x4C,
	/* Version */
	0x41,

	/* COMMANDS */
	//set first sdram
	/* group: 'Imported Commands' */
	/* #1.1-113, command header bytes for merged 'Write - value' command */
	0xCC, 0x03, 0x8C, 0x04, //904=113*8+4
	/* #1.1, command: write_value, address: CCM_CCGR0, value: 0xFFFFFFFF, size: 4 */
	0x40, 0x0F, 0xC0, 0x68, 0xFF, 0xFF, 0xFF, 0xFF,
	/* #1.2, command: write_value, address: CCM_CCGR1, value: 0xFFFFFFFF, size: 4 */
	0x40, 0x0F, 0xC0, 0x6C, 0xFF, 0xFF, 0xFF, 0xFF,
	/* #1.3, command: write_value, address: CCM_CCGR2, value: 0xFFFFFFFF, size: 4 */
	0x40, 0x0F, 0xC0, 0x70, 0xFF, 0xFF, 0xFF, 0xFF,
	/* #1.4, command: write_value, address: CCM_CCGR3, value: 0xFFFFFFFF, size: 4 */
	0x40, 0x0F, 0xC0, 0x74, 0xFF, 0xFF, 0xFF, 0xFF,
	/* #1.5, command: write_value, address: CCM_CCGR4, value: 0xFFFFFFFF, size: 4 */
	0x40, 0x0F, 0xC0, 0x78, 0xFF, 0xFF, 0xFF, 0xFF,
	/* #1.6, command: write_value, address: CCM_CCGR5, value: 0xFFFFFFFF, size: 4 */
	0x40, 0x0F, 0xC0, 0x7C, 0xFF, 0xFF, 0xFF, 0xFF,
	/* #1.7, command: write_value, address: CCM_CCGR6, value: 0xFFFFFFFF, size: 4 */
	0x40, 0x0F, 0xC0, 0x80, 0xFF, 0xFF, 0xFF, 0xFF,
	/* #1.8, command: write_value, address: CCM_ANALOG_PLL_SYS, value: 0x2001, size: 4 */
	0x40, 0x0D, 0x80, 0x30, 0x00, 0x00, 0x20, 0x01,
	/* #1.9, command: write_value, address: CCM_ANALOG_PFD_528, value: 0x1D0000, size: 4 */
	0x40, 0x0D, 0x81, 0x00, 0x00, 0x1D, 0x00, 0x00,
	/* #1.10, command: write_value, address: CCM_CBCDR, value: 0x10D40, size: 4 */
	0x40, 0x0F, 0xC0, 0x14, 0x00, 0x01, 0x0D, 0x40,
	/* #1.11, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_00, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x14, 0x00, 0x00, 0x00, 0x00,
	/* #1.12, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_01, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x18, 0x00, 0x00, 0x00, 0x00,
	/* #1.13, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_02, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x1C, 0x00, 0x00, 0x00, 0x00,
	/* #1.14, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_03, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x20, 0x00, 0x00, 0x00, 0x00,
	/* #1.15, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_04, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x24, 0x00, 0x00, 0x00, 0x00,
	/* #1.16, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_05, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x28, 0x00, 0x00, 0x00, 0x00,
	/* #1.17, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_06, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x2C, 0x00, 0x00, 0x00, 0x00,
	/* #1.18, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_07, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x30, 0x00, 0x00, 0x00, 0x00,
	/* #1.19, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_08, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x34, 0x00, 0x00, 0x00, 0x00,
	/* #1.20, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_09, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x38, 0x00, 0x00, 0x00, 0x00,
	/* #1.21, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_10, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x3C, 0x00, 0x00, 0x00, 0x00,
	/* #1.22, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_11, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x40, 0x00, 0x00, 0x00, 0x00,
	/* #1.23, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_12, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x44, 0x00, 0x00, 0x00, 0x00,
	/* #1.24, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_13, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x48, 0x00, 0x00, 0x00, 0x00,
	/* #1.25, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_14, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x4C, 0x00, 0x00, 0x00, 0x00,
	/* #1.26, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_15, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x50, 0x00, 0x00, 0x00, 0x00,
	/* #1.27, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_16, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x54, 0x00, 0x00, 0x00, 0x00,
	/* #1.28, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_17, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x58, 0x00, 0x00, 0x00, 0x00,
	/* #1.29, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_18, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x5C, 0x00, 0x00, 0x00, 0x00,
	/* #1.30, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_19, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x60, 0x00, 0x00, 0x00, 0x00,
	/* #1.31, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_20, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x64, 0x00, 0x00, 0x00, 0x00,
	/* #1.32, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_21, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x68, 0x00, 0x00, 0x00, 0x00,
	/* #1.33, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_22, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x6C, 0x00, 0x00, 0x00, 0x00,
	/* #1.34, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_23, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x70, 0x00, 0x00, 0x00, 0x00,
	/* #1.35, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_24, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x74, 0x00, 0x00, 0x00, 0x00,
	/* #1.36, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_25, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x78, 0x00, 0x00, 0x00, 0x00,
	/* #1.37, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_26, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x7C, 0x00, 0x00, 0x00, 0x00,
	/* #1.38, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_27, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x80, 0x00, 0x00, 0x00, 0x00,
	/* #1.39, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_28, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x84, 0x00, 0x00, 0x00, 0x00,
	/* #1.40, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_29, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x88, 0x00, 0x00, 0x00, 0x00,
	/* #1.41, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_30, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x8C, 0x00, 0x00, 0x00, 0x00,
	/* #1.42, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_31, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x90, 0x00, 0x00, 0x00, 0x00,
	/* #1.43, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_32, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x94, 0x00, 0x00, 0x00, 0x00,
	/* #1.44, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_33, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x98, 0x00, 0x00, 0x00, 0x00,
	/* #1.45, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_34, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x9C, 0x00, 0x00, 0x00, 0x00,
	/* #1.46, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_35, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0xA0, 0x00, 0x00, 0x00, 0x00,
	/* #1.47, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_36, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0xA4, 0x00, 0x00, 0x00, 0x00,
	/* #1.48, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_37, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0xA8, 0x00, 0x00, 0x00, 0x00,
	/* #1.49, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_38, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0xAC, 0x00, 0x00, 0x00, 0x00,
	/* #1.50, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_39, value: 0x10, size: 4 */
	0x40, 0x1F, 0x80, 0xB0, 0x00, 0x00, 0x00, 0x10,
	/* #1.51, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_00, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x04, 0x00, 0x01, 0x10, 0xF9,
	/* #1.52, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_01, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x08, 0x00, 0x01, 0x10, 0xF9,
	/* #1.53, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_02, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x0C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.54, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_03, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x10, 0x00, 0x01, 0x10, 0xF9,
	/* #1.55, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_04, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x14, 0x00, 0x01, 0x10, 0xF9,
	/* #1.56, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_05, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x18, 0x00, 0x01, 0x10, 0xF9,
	/* #1.57, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_06, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x1C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.58, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_07, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x20, 0x00, 0x01, 0x10, 0xF9,
	/* #1.59, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_08, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x24, 0x00, 0x01, 0x10, 0xF9,
	/* #1.60, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_09, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x28, 0x00, 0x01, 0x10, 0xF9,
	/* #1.61, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_10, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x2C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.62, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_11, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x30, 0x00, 0x01, 0x10, 0xF9,
	/* #1.63, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_12, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x34, 0x00, 0x01, 0x10, 0xF9,
	/* #1.64, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_13, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x38, 0x00, 0x01, 0x10, 0xF9,
	/* #1.65, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_14, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x3C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.66, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_15, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x40, 0x00, 0x01, 0x10, 0xF9,
	/* #1.67, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_16, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x44, 0x00, 0x01, 0x10, 0xF9,
	/* #1.68, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_17, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x48, 0x00, 0x01, 0x10, 0xF9,
	/* #1.69, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_18, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x4C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.70, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_19, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x50, 0x00, 0x01, 0x10, 0xF9,
	/* #1.71, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_20, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x54, 0x00, 0x01, 0x10, 0xF9,
	/* #1.72, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_21, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x58, 0x00, 0x01, 0x10, 0xF9,
	/* #1.73, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_22, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x5C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.74, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_23, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x60, 0x00, 0x01, 0x10, 0xF9,
	/* #1.75, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_24, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x64, 0x00, 0x01, 0x10, 0xF9,
	/* #1.76, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_25, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x68, 0x00, 0x01, 0x10, 0xF9,
	/* #1.77, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_26, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x6C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.78, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_27, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x70, 0x00, 0x01, 0x10, 0xF9,
	/* #1.79, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_28, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x74, 0x00, 0x01, 0x10, 0xF9,
	/* #1.80, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_29, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x78, 0x00, 0x01, 0x10, 0xF9,
	/* #1.81, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_30, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x7C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.82, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_31, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x80, 0x00, 0x01, 0x10, 0xF9,
	/* #1.83, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_32, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x84, 0x00, 0x01, 0x10, 0xF9,
	/* #1.84, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_33, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x88, 0x00, 0x01, 0x10, 0xF9,
	/* #1.85, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_34, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x8C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.86, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_35, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x90, 0x00, 0x01, 0x10, 0xF9,
	/* #1.87, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_36, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x94, 0x00, 0x01, 0x10, 0xF9,
	/* #1.88, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_37, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x98, 0x00, 0x01, 0x10, 0xF9,
	/* #1.89, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_38, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x9C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.90, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_39, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0xA0, 0x00, 0x01, 0x10, 0xF9,
	/* #1.91, command: write_value, address: SEMC_MCR, value: 0x10000004, size: 4 */
	0x40, 0x2F, 0x00, 0x00, 0x10, 0x00, 0x00, 0x04,
	/* #1.92, command: write_value, address: SEMC_BMCR0, value: 0x30524, size: 4 */
	0x40, 0x2F, 0x00, 0x08, 0x00, 0x03, 0x05, 0x24,
	/* #1.93, command: write_value, address: SEMC_BMCR1, value: 0x6030524, size: 4 */
	0x40, 0x2F, 0x00, 0x0C, 0x06, 0x03, 0x05, 0x24,
	/* #1.94, command: write_value, address: SEMC_BR0, value: 0x8000001B, size: 4 */
	0x40, 0x2F, 0x00, 0x10, 0x80, 0x00, 0x00, 0x1B,
	/* #1.95, command: write_value, address: SEMC_BR1, value: 0x8200001B, size: 4 */
	0x40, 0x2F, 0x00, 0x14, 0x82, 0x00, 0x00, 0x1B,
	/* #1.96, command: write_value, address: SEMC_BR2, value: 0x8400001B, size: 4 */
	0x40, 0x2F, 0x00, 0x18, 0x84, 0x00, 0x00, 0x1B,
	/* #1.97, command: write_value, address: SEMC_BR3, value: 0x8600001B, size: 4 */
	0x40, 0x2F, 0x00, 0x1C, 0x8C, 0x00, 0x00, 0x1B,
	/* #1.98, command: write_value, address: SEMC_BR4, value: 0x90000021, size: 4 */
	0x40, 0x2F, 0x00, 0x20, 0x90, 0x00, 0x00, 0x21,
	/* #1.99, command: write_value, address: SEMC_BR5, value: 0xA0000019, size: 4 */
	0x40, 0x2F, 0x00, 0x24, 0xA0, 0x00, 0x00, 0x19,
	/* #1.100, command: write_value, address: SEMC_BR6, value: 0xA8000017, size: 4 */
	0x40, 0x2F, 0x00, 0x28, 0xA8, 0x00, 0x00, 0x17,
	/* #1.101, command: write_value, address: SEMC_BR7, value: 0xA900001B, size: 4 */
	0x40, 0x2F, 0x00, 0x2C, 0xA9, 0x00, 0x00, 0x1B,
	/* #1.102, command: write_value, address: SEMC_BR8, value: 0x21, size: 4 */
	0x40, 0x2F, 0x00, 0x30, 0x00, 0x00, 0x00, 0x21,
	/* #1.103, command: write_value, address: SEMC_IOCR, value: 0x79A8, size: 4 */
	0x40, 0x2F, 0x00, 0x04, 0x00, 0x00, 0x30, 0x00,
	/* #1.104, command: write_value, address: SEMC_SDRAMCR0, value: 0xF31, size: 4 */
	0x40, 0x2F, 0x00, 0x40, 0x00, 0x00, 0x0F, 0x31,
	/* #1.105, command: write_value, address: SEMC_SDRAMCR1, value: 0x652922, size: 4 */
	0x40, 0x2F, 0x00, 0x44, 0x00, 0x66, 0x4B, 0x22,
	/* #1.106, command: write_value, address: SEMC_SDRAMCR2, value: 0x10920, size: 4 */
	0x40, 0x2F, 0x00, 0x48, 0x00, 0x09, 0x09, 0x0B,
	/* #1.107, command: write_value, address: SEMC_SDRAMCR3, value: 0x50210A08, size: 4 */
	0x40, 0x2F, 0x00, 0x4C, 0x08, 0x07, 0x0A, 0x00,
	/* #1.108, command: write_value, address: SEMC_DBICR0, value: 0x21, size: 4 */
	0x40, 0x2F, 0x00, 0x80, 0x00, 0x00, 0x00, 0x21,
	/* #1.109, command: write_value, address: SEMC_DBICR1, value: 0x888888, size: 4 */
	0x40, 0x2F, 0x00, 0x84, 0x00, 0x88, 0x88, 0x88,
	/* #1.110, command: write_value, address: SEMC_IPCR1, value: 0x02, size: 4 */
	0x40, 0x2F, 0x00, 0x94, 0x00, 0x00, 0x00, 0x02,
	/* #1.111, command: write_value, address: SEMC_IPCR2, value: 0x00, size: 4 */
	0x40, 0x2F, 0x00, 0x98, 0x00, 0x00, 0x00, 0x00,
	/* #1.112, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */
	0x40, 0x2F, 0x00, 0x90, 0x80, 0x00, 0x00, 0x00,
	/* #1.113, command: write_value, address: SEMC_IPCMD, value: 0xA55A000F, size: 4 */
	0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0F,
	/* #2, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
	0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
	/* #3.1-2, command header bytes for merged 'Write - value' command */
	0xCC, 0x00, 0x14, 0x04,
	/* #3.1, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */
	0x40, 0x2F, 0x00, 0x90, 0x80, 0x00, 0x00, 0x00,
	/* #3.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */
	0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,
	/* #4, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
	0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
	/* #5.1-2, command header bytes for merged 'Write - value' command */
	0xCC, 0x00, 0x14, 0x04,
	/* #5.1, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */
	0x40, 0x2F, 0x00, 0x90, 0x80, 0x00, 0x00, 0x00,
	/* #5.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */
	0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,
	/* #6, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
	0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
	/* #7.1-3, command header bytes for merged 'Write - value' command */
	0xCC, 0x00, 0x1C, 0x04,
	/* #7.1, command: write_value, address: SEMC_IPTXDAT, value: 0x33, size: 4 */
	0x40, 0x2F, 0x00, 0xA0, 0x00, 0x00, 0x00, 0x33,
	/* #7.2, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */
	0x40, 0x2F, 0x00, 0x90, 0x80, 0x00, 0x00, 0x00,
	/* #7.3, command: write_value, address: SEMC_IPCMD, value: 0xA55A000A, size: 4 */
	0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0A,
	/* #8, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
	0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
	/* #9, command: write_value, address: SEMC_SDRAMCR3, value: 0x50210A09, size: 4 */
	0xCC, 0x00, 0x0C, 0x04, 0x40, 0x2F, 0x00, 0x4C, 0x08, 0x07, 0x0A, 0x01,
	//1040bytes

	//set second sdram
	0xCC, 0x00, 0xBC, 0x04, //188=23*8+4
	/* #1.91, command: write_value, address: SEMC_MCR, value: 0x10000004, size: 4 */
	0x40, 0x2F, 0x00, 0x00, 0x10, 0x00, 0x00, 0x04,
	/* #1.92, command: write_value, address: SEMC_BMCR0, value: 0x30524, size: 4 */
	0x40, 0x2F, 0x00, 0x08, 0x00, 0x03, 0x05, 0x24,
	/* #1.93, command: write_value, address: SEMC_BMCR1, value: 0x6030524, size: 4 */
	0x40, 0x2F, 0x00, 0x0C, 0x06, 0x03, 0x05, 0x24,
	/* #1.94, command: write_value, address: SEMC_BR0, value: 0x8000001B, size: 4 */
	0x40, 0x2F, 0x00, 0x10, 0x80, 0x00, 0x00, 0x1B,
	/* #1.95, command: write_value, address: SEMC_BR1, value: 0x8200001B, size: 4 */
	0x40, 0x2F, 0x00, 0x14, 0x82, 0x00, 0x00, 0x1B,
	/* #1.96, command: write_value, address: SEMC_BR2, value: 0x8400001B, size: 4 */
	0x40, 0x2F, 0x00, 0x18, 0x84, 0x00, 0x00, 0x1B,
	/* #1.97, command: write_value, address: SEMC_BR3, value: 0x8600001B, size: 4 */
	0x40, 0x2F, 0x00, 0x1C, 0x8C, 0x00, 0x00, 0x1B,
	/* #1.98, command: write_value, address: SEMC_BR4, value: 0x90000021, size: 4 */
	0x40, 0x2F, 0x00, 0x20, 0x90, 0x00, 0x00, 0x21,
	/* #1.99, command: write_value, address: SEMC_BR5, value: 0xA0000019, size: 4 */
	0x40, 0x2F, 0x00, 0x24, 0xA0, 0x00, 0x00, 0x19,
	/* #1.100, command: write_value, address: SEMC_BR6, value: 0xA8000017, size: 4 */
	0x40, 0x2F, 0x00, 0x28, 0xA8, 0x00, 0x00, 0x17,
	/* #1.101, command: write_value, address: SEMC_BR7, value: 0xA900001B, size: 4 */
	0x40, 0x2F, 0x00, 0x2C, 0xA9, 0x00, 0x00, 0x1B,
	/* #1.102, command: write_value, address: SEMC_BR8, value: 0x21, size: 4 */
	0x40, 0x2F, 0x00, 0x30, 0x00, 0x00, 0x00, 0x21,
	/* #1.103, command: write_value, address: SEMC_IOCR, value: 0x79A8, size: 4 */
	0x40, 0x2F, 0x00, 0x04, 0x00, 0x00, 0x30, 0x00,
	/* #1.104, command: write_value, address: SEMC_SDRAMCR0, value: 0xF31, size: 4 */
	0x40, 0x2F, 0x00, 0x40, 0x00, 0x00, 0x0F, 0x31,
	/* #1.105, command: write_value, address: SEMC_SDRAMCR1, value: 0x652922, size: 4 */
	0x40, 0x2F, 0x00, 0x44, 0x00, 0x66, 0x4B, 0x22,
	/* #1.106, command: write_value, address: SEMC_SDRAMCR2, value: 0x10920, size: 4 */
	0x40, 0x2F, 0x00, 0x48, 0x00, 0x09, 0x09, 0x0B,
	/* #1.107, command: write_value, address: SEMC_SDRAMCR3, value: 0x50210A08, size: 4 */
	0x40, 0x2F, 0x00, 0x4C, 0x08, 0x07, 0x0A, 0x00,
	/* #1.108, command: write_value, address: SEMC_DBICR0, value: 0x21, size: 4 */
	0x40, 0x2F, 0x00, 0x80, 0x00, 0x00, 0x00, 0x21,
	/* #1.109, command: write_value, address: SEMC_DBICR1, value: 0x888888, size: 4 */
	0x40, 0x2F, 0x00, 0x84, 0x00, 0x88, 0x88, 0x88,
	/* #1.110, command: write_value, address: SEMC_IPCR1, value: 0x02, size: 4 */
	0x40, 0x2F, 0x00, 0x94, 0x00, 0x00, 0x00, 0x02,
	/* #1.111, command: write_value, address: SEMC_IPCR2, value: 0x00, size: 4 */
	0x40, 0x2F, 0x00, 0x98, 0x00, 0x00, 0x00, 0x00,
	/* #1.112, command: write_value, address: SEMC_IPCR0, value: 0x8C000000, size: 4 */
	0x40, 0x2F, 0x00, 0x90, 0x8C, 0x00, 0x00, 0x00,
	/* #1.113, command: write_value, address: SEMC_IPCMD, value: 0xA55A000F, size: 4 */
	0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0F,
    /* #4, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
    0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
    /* #5.1-2, command header bytes for merged 'Write - value' command */
    0xCC, 0x00, 0x14, 0x04,
    /* #5.1, command: write_value, address: SEMC_IPCR0, value: 0x8C000000, size: 4 */
    0x40, 0x2F, 0x00, 0x90, 0x8C, 0x00, 0x00, 0x00,
    /* #3.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */
    0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,
    /* #4, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
    0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
    /* #5.1-2, command header bytes for merged 'Write - value' command */
    0xCC, 0x00, 0x14, 0x04,
    /* #5.1, command: write_value, address: SEMC_IPCR0, value: 0x8C000000, size: 4 */
    0x40, 0x2F, 0x00, 0x90, 0x8C, 0x00, 0x00, 0x00,
    /* #5.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */
    0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,
    /* #6, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
    0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
    /* #7.1-3, command header bytes for merged 'Write - value' command */
    0xCC, 0x00, 0x1C, 0x04,
    /* #7.1, command: write_value, address: SEMC_IPTXDAT, value: 0x33, size: 4 */
    0x40, 0x2F, 0x00, 0xA0, 0x00, 0x00, 0x00, 0x33,
    /* #7.2, command: write_value, address: SEMC_IPCR0, value: 0x8C000000, size: 4 */
    0x40, 0x2F, 0x00, 0x90, 0x8C, 0x00, 0x00, 0x00,
    /* #7.3, command: write_value, address: SEMC_IPCMD, value: 0xA55A000A, size: 4 */
    0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0A,
    /* #8, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
    0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
    /* #9, command: write_value, address: SEMC_SDRAMCR3, value: 0x50210A09, size: 4 */
	0xCC, 0x00, 0x0C, 0x04, 0x40, 0x2F, 0x00, 0x4C, 0x08, 0x07, 0x0A, 0x01};
/* BE CAREFUL MODIFYING THIS SETTINGS - IT IS YAML SETTINGS FOR TOOLS */
//316 bytes
#else
const uint8_t dcd_data[] = {0x00};
#endif /* XIP_BOOT_HEADER_DCD_ENABLE */
#endif /* XIP_BOOT_HEADER_ENABLE */

 

Best regards,

Doris

0 Kudos
Reply
1 Solution
2,886 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @MCW ,

Yes, you can enable two SDRAM in dcd. The RT1170 EVK has two SDRAM too, and they are initialized in DCD. It is needn't to write many SEMC register twice in DCD. You can refer to the dcd file in RT1170 SDK examples.

 

Regards,

Jing

View solution in original post

4 Replies
2,862 Views
MCW
Contributor III

Hi @jingpan ,

 

Thanks for your reply.

It works after I add this code which is related to set  IOMUXC_GPIO_B0_02_SEMC_CSX03 in the dcd.c

0x40, 0x1F, 0x81, 0x44, 0x00, 0x00, 0x00, 0x06,
0x40, 0x1F, 0x83, 0x34, 0x00, 0x01, 0x10, 0xF9,

 

Best regards,

Doris

0 Kudos
Reply
2,887 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @MCW ,

Yes, you can enable two SDRAM in dcd. The RT1170 EVK has two SDRAM too, and they are initialized in DCD. It is needn't to write many SEMC register twice in DCD. You can refer to the dcd file in RT1170 SDK examples.

 

Regards,

Jing

2,852 Views
MCW
Contributor III

Hi @jingpan ,

 

I have one more question. I used the default dcd.c which IOCR defualt value is 0x79A8. And then I applied SEMC_ConfigureSDRAM function to set two sdrams. The read/write result of the second SDRAM was wrong. However, the read/write result was correct when I set the value of IOCR as 0x39A8 in the dcd.c. I have checked the datasheet, 15-17 bits of IOCR register are used for SEMC_RDY function selection. For my customize board, I don't use the SEMC_RDY pin because it is assigned for other gpio function.

Why setting MUX_RDY to 001 has some impacts on the second sdram read/write?

IOCR_datasheet.png

Best regards.

Doris 

0 Kudos
Reply
2,841 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @MCW ,

To MUX_RDY field, 0x00079a8 is same to 0x00039a8. It is bit 17~15, all zero. What different is MUX_CSX3.

 

Regards,

Jing

0 Kudos
Reply