Content in imx93 timer is not executed.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Content in imx93 timer is not executed.

Jump to solution
286 Views
xiang_1001
Contributor III

bsp:real-time-edge-3.1.0.xml

The /etc/net-debug.sh file is executed regularly in /etc/crontab, but now this script doesn't run. What is the reason?

xiang_1001_0-1759204650814.png

 

0 Kudos
Reply
1 Solution
254 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Common Reasons for a Failed Cron Job

 

 

  • Permissions: The script lacks execute permissions. You need to make the script executable using chmod +x /path/to/your/script.sh.
  • Path Environment Variable: Cron runs scripts in a minimal environment with a restricted PATH. Commands within the script may not be found.

 

 

  • Missing or Incorrect Paths:
    • The crontab entry itself might use relative paths, which is problematic for cron.
    • The script might not specify the full path to commands it calls (e.g., instead of ls, use /bin/ls).
  • Crontab Syntax Errors:
    • There must be a newline character after the last command in the crontab file.
    • The user field is missing in the /etc/crontab file, which requires a user name before the command.
  •   Issues:
    • The script may rely on environment variables that are not set in the minimal cron environment.
    • Scripts containing non-text characters can cause failures

 

Troubleshooting Steps
 
  1. Log Script Output: Redirect the script's output to a log file to see any error messages.
    bash

  • * * * * * /path/to/your/script.sh >> /var/log/your_script.log 2>&1
    
  • Check Permissions: Use ls -l /path/to/your/script.sh to verify the script has execute (x) permissions. If not, run chmod +x /path/to/your/script.sh.
  • Use Full Paths: In your script, replace relative path commands with their full paths (e.g., /bin/grep instead of grep).
  • Set Environment Variables: Add PATH and other necessary variables at the top of your cron entry or script to define the environment.
  • Check for Newline: Open /etc/crontab and ensure there is a new line character after the last command in your entry.
  • Verify User Field: For /etc/crontab, ensure the user field is present (e.g., root).
  • Use cron.d: For root-owned jobs, consider placing them in /etc/cron.d/ instead of directly editing /etc/crontab for better organization

Regards

View solution in original post

0 Kudos
Reply
2 Replies
255 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Common Reasons for a Failed Cron Job

 

 

  • Permissions: The script lacks execute permissions. You need to make the script executable using chmod +x /path/to/your/script.sh.
  • Path Environment Variable: Cron runs scripts in a minimal environment with a restricted PATH. Commands within the script may not be found.

 

 

  • Missing or Incorrect Paths:
    • The crontab entry itself might use relative paths, which is problematic for cron.
    • The script might not specify the full path to commands it calls (e.g., instead of ls, use /bin/ls).
  • Crontab Syntax Errors:
    • There must be a newline character after the last command in the crontab file.
    • The user field is missing in the /etc/crontab file, which requires a user name before the command.
  •   Issues:
    • The script may rely on environment variables that are not set in the minimal cron environment.
    • Scripts containing non-text characters can cause failures

 

Troubleshooting Steps
 
  1. Log Script Output: Redirect the script's output to a log file to see any error messages.
    bash

  • * * * * * /path/to/your/script.sh >> /var/log/your_script.log 2>&1
    
  • Check Permissions: Use ls -l /path/to/your/script.sh to verify the script has execute (x) permissions. If not, run chmod +x /path/to/your/script.sh.
  • Use Full Paths: In your script, replace relative path commands with their full paths (e.g., /bin/grep instead of grep).
  • Set Environment Variables: Add PATH and other necessary variables at the top of your cron entry or script to define the environment.
  • Check for Newline: Open /etc/crontab and ensure there is a new line character after the last command in your entry.
  • Verify User Field: For /etc/crontab, ensure the user field is present (e.g., root).
  • Use cron.d: For root-owned jobs, consider placing them in /etc/cron.d/ instead of directly editing /etc/crontab for better organization

Regards

0 Kudos
Reply
180 Views
xiang_1001
Contributor III
I can use the timing function by putting the crontab file into the /etc/cron.d/ file.
0 Kudos
Reply