Connection between IMIX7D and LPDDR3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connection between IMIX7D and LPDDR3

Jump to solution
1,528 Views
goto11
Contributor III

Hello,Community

About the attached file "LPDDR3 connection for i.MX7D.xlsx" at https://community.nxp.com/message/829534
Is the following signal correct in the IMX7D and LPDDR3 connection signal correspondence table?


IMX7D                      >>>>>    LPDDR3 (x32 DDP)
DRAM_SDCLK0_N >>>>>     CK
DRAM_SDCLK0_P >>>>>     /CK

best regards

Goto

Labels (1)
0 Kudos
Reply
1 Solution
1,466 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

It should be:

IMX7D                          LPDDR3
DRAM_SDCLK0_N      /CK
DRAM_SDCLK0_P       CK

 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

View solution in original post

0 Kudos
Reply
1 Reply
1,467 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

It should be:

IMX7D                          LPDDR3
DRAM_SDCLK0_N      /CK
DRAM_SDCLK0_P       CK

 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply