Connecting to multiple servers from a client in BLE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Connecting to multiple servers from a client in BLE

26,225 次查看
EmbeddedTech
Contributor III

Hi,

I am trying to connect my BLE Client (iMXRT1060 +ublox module) with 2 servers (QN9090). I was able to successfully connect to one board and read the data. When I try to establish connection with both the servers only one gets connected and for the other module I get the error as below,

Found device:
Create connection failed (err -12)

I have configured the CONFIG_BT_MAX_CONN to 2 and have done the required modifications in the central_ht.c file to connect to 2 servers. But I understand from the above error that the SDK currently supports only one connection. Is that correct?

Is there any sample SDK to connect to multiple servers as we need to connect to multiple peripherals to get data. Your help on this is highly appreciated.

Thanks.

 

0 项奖励
回复
16 回复数

26,168 次查看
EmbeddedTech
Contributor III

Hi Kerry,

Ok, I will wait for your reply.

Thanks.

0 项奖励
回复

26,153 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @EmbeddedTech 

  nxf56274 is my BLE colleague, he helps you test it today, please follow his code and test it on your side, whether it works or not?

 Any updated information, please kindly let me know.

Best Regards,

Kerry

0 项奖励
回复

26,145 次查看
EmbeddedTech
Contributor III

Hi Kerry,

I will update on my side and test it today.

Thanks.

0 项奖励
回复

26,201 次查看
EmbeddedTech
Contributor III

Hi,

Our requirement is to connect to multiple servers (atleast 3) to get the data. Since BLE can support a maximum of 7 connections at a time, should the sdk also support multiple connections? Can you help us with the changes to be done on the sdk side to support multiple connections?

Thanks.

0 项奖励
回复

26,192 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @EmbeddedTech 

   Sorry, my previous reply is not correct, I checked with our BLE engineer, the client can connect more than 2 server at the same time.

  Please refer to this application note at first:

https://www.nxp.com/docs/en/application-note/AN12414.pdf

 If you still have question about it please kindly let me know.

Best Regards,

Kerry

  

0 项奖励
回复

26,185 次查看
EmbeddedTech
Contributor III

Hi Kerry,

Does the edgefast bluetooth example in iMXRT 1060 SDK support multiple connections? I am using the ublox module so I have defined the macro WIFI_BOARD_AW_CM358. The sdk code for edgefast bluetooth is different from the freedom series code. 

I have defined the macro CONFIG_BT_MAX_CONN to 2 and have also done changes in the central_ht.c file to support 2 connections. But looks like I can establish only one connection at a time.

In file bluetooth.h, what does the below macro mean?

/**
* @def BT_ID_DEFAULT
*
* Convenience macro for specifying the default identity. This helps
* make the code more readable, especially when only one identity is
* supported.
*/
#define BT_ID_DEFAULT 0

The above ID is used in bt_pal_conn.c etc. Does this mean the sdk currently supports only one connection?

Your help on this is highly appreciated.

Thanks.

0 项奖励
回复

26,132 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

I wrote a code but I do not have the device. So I hope you can test it. I am trying to use the array to store the connection info. 

nxf56274_0-1639991403244.png

 

0 项奖励
回复

26,110 次查看
EmbeddedTech
Contributor III

Hi,

I have tested the code and it is asserting after subscribing to one service. Please find attached the screenshots for your reference.

Thanks.

0 项奖励
回复

26,100 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

1 Comment the 'scan_start', Does it work with only one device?

asd1.PNG

2 If so, please try to create a thread. In the thread, the uart is waiting for the cmd to call the scan_start after the first device sending the data normally.

0 项奖励
回复

26,095 次查看
EmbeddedTech
Contributor III

Hi,

Do you mean like setting some sort of flag in the notify function on first receive and then use the flag in a new task to start scanning again?

0 项奖励
回复

26,084 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Yeah, this method works on kw. So I want you to try.

0 项奖励
回复

26,082 次查看
EmbeddedTech
Contributor III

Hi,

Please find attached the file and the screenshot. Let me know if it makes sense. I will do some more testing to see if its consistent and will also do changes to my custom peripherals read to see if it works.

Thanks.

26,076 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Yeah, it looks good 

0 项奖励
回复

25,676 次查看
EmbeddedTech
Contributor III

Hi,

Good morning. Now, I am trying to connect a third peripheral to my central device and I am able to establish a connection after connecting and subscribing to the first two peripherals. But after connecting the service discovery fails. The error code is 12 (ENOMEM). What does that mean?

Thanks.

0 项奖励
回复

25,648 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

 

I will no longer support the wireless mcu. If you have any other question, please create a new thread. Many thanks.

 

BR,

Da

0 项奖励
回复

26,145 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @EmbeddedTech 

  Please keep patient, I will find more resource to check the details, any updated information will let you know, please give me more time, thanks.

Best Regards,

kerry

0 项奖励
回复