/* * Copyright (c) 2020 SixOctets Systems * Copyright 2021 NXP * * SPDX-License-Identifier: Apache-2.0 */ #include #include #include #include #include #include #include #include #include #include #include #include #include /******************************************************************************* * Prototypes ******************************************************************************/ static int scan_start(void); /******************************************************************************* * Definitions ******************************************************************************/ #define CONN_DEVICE 3 static struct bt_conn *default_conn[CONN_DEVICE]; static struct bt_uuid_16 uuid = BT_UUID_INIT_16(0); static struct bt_gatt_discover_params discover_params[CONN_DEVICE]; static struct bt_gatt_subscribe_params subscribe_params[CONN_DEVICE]; /******************************************************************************* * Code ******************************************************************************/ static uint8_t notify_func(struct bt_conn *conn, struct bt_gatt_subscribe_params *params, const void *data, uint16_t length) { struct temp_measurement temp_measurement; uint32_t temperature; if (!data) { PRINTF("Unsubscribed \n"); params->value_handle = 0U; return BT_GATT_ITER_STOP; } /* temperature value display */ temp_measurement = *(struct temp_measurement*)data; temperature = sys_get_le32(temp_measurement.temperature); if ((temp_measurement.flags & BIT0) == hts_unit_celsius_c) { PRINTF("Temperature %d degrees Celsius \n", temperature); } else { PRINTF("Temperature %d degrees Fahrenheit \n", temperature); } return BT_GATT_ITER_CONTINUE; } static uint8_t discover_func(struct bt_conn *conn, const struct bt_gatt_attr *attr, struct bt_gatt_discover_params *params) { int32_t err; if (!attr) { PRINTF("Discover complete, No attribute found \n"); (void)memset(params, 0, sizeof(*params)); scan_start(); return BT_GATT_ITER_STOP; } for(uint32_t i=0; ihandle + 1; discover_params[i].type = BT_GATT_DISCOVER_CHARACTERISTIC; err = bt_gatt_discover(conn, &discover_params[i]); if (err) { PRINTF("Discover failed (err %d)\n", err); } } else if (bt_uuid_cmp(discover_params[i].uuid, BT_UUID_HTS_MEASUREMENT) == 0) { /* Health Thermometer Measurement characteristic discovered */ memcpy(&uuid, BT_UUID_GATT_CCC, sizeof(uuid)); discover_params[i].uuid = &uuid.uuid; discover_params[i].start_handle = attr->handle + 2; discover_params[i].type = BT_GATT_DISCOVER_DESCRIPTOR; subscribe_params[i].value_handle = bt_gatt_attr_value_handle(attr); err = bt_gatt_discover(conn, &discover_params[i]); if (err) { PRINTF("Discover failed (err %d)\n", err); } } else { /* Subscribe to Health Thermometer service */ subscribe_params[i].notify = notify_func; subscribe_params[i].value = BT_GATT_CCC_INDICATE; subscribe_params[i].ccc_handle = attr->handle; err = bt_gatt_subscribe(conn, &subscribe_params[i]); if (err && err != -EALREADY) { PRINTF("Subscribe failed (err %d)\n", err); } else { PRINTF("Subscribed to HTS\n"); scan_start(); } return BT_GATT_ITER_STOP; } break; } } return BT_GATT_ITER_STOP; } static void connected(struct bt_conn *conn, uint8_t conn_err) { char addr[BT_ADDR_LE_STR_LEN]; int32_t err; bt_addr_le_to_str(bt_conn_get_dst(conn), addr, sizeof(addr)); if (conn_err) { PRINTF("Failed to connect to %s (err %u)\n", addr, conn_err); for(uint32_t i=0; itype) { case BT_DATA_UUID16_SOME: case BT_DATA_UUID16_ALL: { if (data->data_len % sizeof(uint16_t) != 0U) { PRINTF("AD malformed\n"); return true; } for (i = 0; i < data->data_len; i += sizeof(uint16_t)) { memcpy(&u16, &data->data[i], sizeof(u16)); uuid = BT_UUID_DECLARE_16(sys_le16_to_cpu(u16)); /* search for the HTS UUID in the advertising data */ if (bt_uuid_cmp(uuid, BT_UUID_HTS) == 0) { /* found the temperature server - stop scanning */ err = bt_le_scan_stop(); if (err) { PRINTF("Stop LE scan failed (err %d)\n", err); break; } PRINTF("Found device: %s", addr); for(uint32_t i=0; ilen, rssi); /* We're only interested in connectable events */ if (type == BT_GAP_ADV_TYPE_ADV_IND || type == BT_GAP_ADV_TYPE_ADV_DIRECT_IND) { bt_data_parse(ad, device_scanned, (void *)addr); } } static int scan_start(void) { struct bt_le_scan_param scan_param = { .type = BT_LE_SCAN_TYPE_PASSIVE, .options = BT_LE_SCAN_OPT_NONE, .interval = BT_GAP_SCAN_FAST_INTERVAL, .window = BT_GAP_SCAN_FAST_WINDOW, }; return bt_le_scan_start(&scan_param, device_found); } static void disconnected(struct bt_conn *conn, uint8_t reason) { // int32_t err; // // PRINTF("Disconnected reason 0x%02x\n", reason); // // if (default_conn != conn) // { // return; // } // // bt_conn_unref(default_conn); // default_conn = NULL; // // /* Restart scanning */ // err = scan_start(); // if (err) // { // PRINTF("Scanning failed to start (err %d)\n", err); // } // else // { // PRINTF("Scanning started\n"); // } } #if CONFIG_BT_SMP static void security_changed(struct bt_conn *conn, bt_security_t level, enum bt_security_err err) { char addr[BT_ADDR_LE_STR_LEN]; bt_addr_le_to_str(bt_conn_get_dst(conn), addr, sizeof(addr)); PRINTF("Security changed: %s level %u (error %d)\n", addr, level, err); } static void auth_passkey_display(struct bt_conn *conn, unsigned int passkey) { char addr[BT_ADDR_LE_STR_LEN]; bt_addr_le_to_str(bt_conn_get_dst(conn), addr, sizeof(addr)); PRINTF("Passkey for %s: %06u\n", addr, passkey); } static void auth_cancel(struct bt_conn *conn) { char addr[BT_ADDR_LE_STR_LEN]; bt_addr_le_to_str(bt_conn_get_dst(conn), addr, sizeof(addr)); PRINTF("Pairing cancelled: %s\n", addr); } #endif static struct bt_conn_cb conn_callbacks = { .connected = connected, .disconnected = disconnected, #if CONFIG_BT_SMP .security_changed = security_changed, #endif }; #if CONFIG_BT_SMP static struct bt_conn_auth_cb auth_cb_display = { .passkey_display = auth_passkey_display, .passkey_entry = NULL, .cancel = auth_cancel, }; #endif static void bt_ready(int err) { if (err) { PRINTF("Bluetooth init failed (err %d)\n", err); return; } if (IS_ENABLED(CONFIG_BT_SETTINGS)) { settings_load(); } PRINTF("Bluetooth initialized\n"); /* Register connection callback */ bt_conn_cb_register(&conn_callbacks); #if CONFIG_BT_SMP bt_conn_auth_cb_register(&auth_cb_display); #endif /* Start scanning */ err = scan_start(); if (err) { PRINTF("Scanning failed to start (err %d)\n", err); return; } PRINTF("Scanning started\n"); } void central_ht_task(void *pvParameters) { int err; err = bt_enable(bt_ready); if (err) { PRINTF("Bluetooth init failed (err %d)\n", err); while (1) { vTaskDelay(2000); } } while (1) { vTaskDelay(1000); } }