Connecting MIPI-CSI2 to custom FPGA camera front end without D-PHY on either side?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connecting MIPI-CSI2 to custom FPGA camera front end without D-PHY on either side?

1,166 Views
dehuanxin
Contributor III

Hi, everyone,

I'm trying to design a system that uses FPGA as digital front end and use MIPI-CSI2 to receive data on IMX6.

The connection of the two is short and is on the same PCB. And the connection does not to be completely MIPI-CSI2 compliant.

Is it possible and recommended to connect IMX6 to the FPGA directly via MIPI-CSI2 without D-PHY in between?

Labels (2)
0 Kudos
Reply
1 Reply

896 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dehuan

seems this is possible, however electrical specifications given in

sect.4.11.12 MIPI D-PHY i.MX6DQ Datasheet (rev.4, 7/2015) should be observed

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply