Configuring the address pins of 8-bit SDRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuring the address pins of 8-bit SDRAM

Jump to solution
1,538 Views
sowmiya_a
Contributor I

Hi,

In evaluation board of i.MXRT1024, a 16-bit SDRAM (IS42S16160J-6TLI )is interfaced to controller. In that, Address lines are configured from A0 to A13.

We are using MIMXRT1024CAG4B and planning to interface a 8-bit SDRAM (IS42S86400F-7TLI) in our design. Can I configure the address pins of 8-bit SDRAM from A0 or is there any specific constraints in configuring these address pins?

sowmiya_a_1-1682511691225.png

 

 

Labels (1)
0 Kudos
Reply
1 Solution
1,501 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Yes, this is correct.

View solution in original post

0 Kudos
Reply
3 Replies
1,502 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Yes, this is correct.

0 Kudos
Reply
1,516 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @sowmiya_a,

The connection are OK, except for the DQM pin. For 8bit SDRAM, SEMC_DM0 (GPIO_EMC_08) should be used, and SEMC_DM1 (GPIO_EMC_31) should be left unconnected.

BR,
Edwin.

0 Kudos
Reply
1,508 Views
sowmiya_a
Contributor I

Hi Edwin,

Thanks for the response.

I will modify the connection of DQM pin. Based on your response, it seems like the configuration of the address pins of the 8-bit SDRAM is correct. Can you confirm if my understanding is correct?

Regards,

Sowmiya

0 Kudos
Reply