Configuring the address pins of 8-bit SDRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Configuring the address pins of 8-bit SDRAM

跳至解决方案
1,527 次查看
sowmiya_a
Contributor I

Hi,

In evaluation board of i.MXRT1024, a 16-bit SDRAM (IS42S16160J-6TLI )is interfaced to controller. In that, Address lines are configured from A0 to A13.

We are using MIMXRT1024CAG4B and planning to interface a 8-bit SDRAM (IS42S86400F-7TLI) in our design. Can I configure the address pins of 8-bit SDRAM from A0 or is there any specific constraints in configuring these address pins?

sowmiya_a_1-1682511691225.png

 

 

标签 (1)
0 项奖励
回复
1 解答
1,490 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Yes, this is correct.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,491 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Yes, this is correct.

0 项奖励
回复
1,505 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @sowmiya_a,

The connection are OK, except for the DQM pin. For 8bit SDRAM, SEMC_DM0 (GPIO_EMC_08) should be used, and SEMC_DM1 (GPIO_EMC_31) should be left unconnected.

BR,
Edwin.

0 项奖励
回复
1,497 次查看
sowmiya_a
Contributor I

Hi Edwin,

Thanks for the response.

I will modify the connection of DQM pin. Based on your response, it seems like the configuration of the address pins of the 8-bit SDRAM is correct. Can you confirm if my understanding is correct?

Regards,

Sowmiya

0 项奖励
回复