Configuring SD card on SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuring SD card on SPI

Jump to solution
1,773 Views
deepika_t
Contributor IV

Hi Everyone,

We are planning to create a custom i.mx6 board with SD card on SPI. We will be using Android 6 as the Operating system.This SD card will not be used for booting but just for external memory.

Is this  possible? Also what would be the maximum capacity of the SD Card it would support.

If this is possible  then do we have device tree configuration for this.

Thanks and Regards,

Deepika

0 Kudos
Reply
1 Solution
1,716 Views
igorpadykov
NXP Employee
NXP Employee

Hi Deepika

seems SD card on SPI is not supported as shown on below part of document

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,716 Views
deepika_t
Contributor IV

Thanks a lot Igor for a quick reply. We need to check for SDIO again

0 Kudos
Reply
1,717 Views
igorpadykov
NXP Employee
NXP Employee

Hi Deepika

seems SD card on SPI is not supported as shown on below part of document

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply