Configuring SD card on SPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuring SD card on SPI

ソリューションへジャンプ
1,767件の閲覧回数
deepika_t
Contributor IV

Hi Everyone,

We are planning to create a custom i.mx6 board with SD card on SPI. We will be using Android 6 as the Operating system.This SD card will not be used for booting but just for external memory.

Is this  possible? Also what would be the maximum capacity of the SD Card it would support.

If this is possible  then do we have device tree configuration for this.

Thanks and Regards,

Deepika

0 件の賞賛
返信
1 解決策
1,710件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Deepika

seems SD card on SPI is not supported as shown on below part of document

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,710件の閲覧回数
deepika_t
Contributor IV

Thanks a lot Igor for a quick reply. We need to check for SDIO again

0 件の賞賛
返信
1,711件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Deepika

seems SD card on SPI is not supported as shown on below part of document

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信