Hello,
I wish to configure QT5.3.2 with X11 on imx6 solo based custom platform. I followed the steps on
http://wiki.wandboard.org/Integrate_Qt5_into_yocto_sato_image_on_Wandboard .
The build goes through but qt applications with qml give errors like : Unable to find an X11 visual which matches EGL config 28
I have also confirmed that Force egl visual ID 33.patch is also getting applied.
Any suggestions would be of help.
Thanks,
Chaitanya D
 
					
				
		
 jimmychan
		
			jimmychan
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
I tried this patch. Its not getting applied. Its failing in do_patch(). In qt 5.3.2, we do not have a "egl" folder under "src/gui/". Sine the patch tries to make changes in the path /src/giu/egl/qegl_x11.cpp which is not existant, it is failing.
Any more help will be appreciated.
Thanks,
Chaitanya Dhere
 
					
				
		
 jimmychan
		
			jimmychan
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		I think if the error still exist, you may try to find the string "Unable to find an X11 visual which matches EGL" in the source code. Then modify the return ID to 33.