Configure fails for nativesdk-alsa-lib.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configure fails for nativesdk-alsa-lib.

44,911 Views
bryan_prather
Contributor II

I get the following errors when building meta-toolchain-qt5 with the latest from https://github.com/mahyar-ym/boundary-community-bsp-base

meta-qt5 is using qt 5.3.

I've attached the files bblayers.conf and local.confg.

 

Copyright (C) 2014 Free Software Foundation, Inc.

This is free software; see the source for copying conditions.  There is NO

warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

 

 

configure:3475: $? = 0

configure:3464: i686-pokysdk-linux-gcc -march=i686 --sysroot=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/cortexa9hf-vfp-neon-mx6-pokysdk-linux -v >&5

Using built-in specs.

COLLECT_GCC=i686-pokysdk-linux-gcc

COLLECT_LTO_WRAPPER=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/lto-wrapper

Target: i686-pokysdk-linux

Configured with: /home/opti/sandbox/mahyar-ym/build/tmp/work-shared/gcc-4.9.1-r0/gcc-4.9.1/configure --build=x86_64-linux --host=x86_64-linux --target=i686-pokysdk-linux --prefix=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr --exec_prefix=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr --bindir=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/bin/i686-pokysdk-linux --sbindir=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/bin/i686-pokysdk-linux --libexecdir=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/libexec/i686-pokysdk-linux --datadir=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/share --sysconfdir=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/etc --sharedstatedir=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/com --localstatedir=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/var --libdir=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/lib/i686-pokysdk-linux --includedir=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/include --oldincludedir=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/include --infodir=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/share/info --mandir=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/share/man --disable-silent-rules --disable-dependency-tracking --with-libtool-sysroot=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux --enable-clocale=generic --with-gnu-ld --enable-shared --enable-languages=c,c++ --enable-threads=posix --disable-multilib --enable-c99 --enable-long-long --enable-symvers=gnu --enable-libstdcxx-pch --program-prefix=i686-pokysdk-linux- --without-local-prefix --enable-target-optspace --enable-lto --enable-libssp --disable-bootstrap --disable-libmudflap --with-system-zlib --with-linker-hash-style=gnu --enable-linker-build-id --with-ppl=no --with-cloog=no --enable-checking=release --enable-cheaders=c_global --with-gxx-include-dir=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/i686-nativesdk-pokysdk-linux/opt/poky/1.6+snapshot/sysroots/i686-pokysdk-linux/usr/include/c++/4.9.1 --with-sysroot=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/i686-nativesdk-pokysdk-linux --with-build-sysroot=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/i686-nativesdk-pokysdk-linux --enable-poison-system-directories --with-mpfr=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr --with-system-zlib --disable-nls --enable-__cxa_atexit

Thread model: posix

gcc version 4.9.1 (GCC)

configure:3475: $? = 0

configure:3464: i686-pokysdk-linux-gcc -march=i686 --sysroot=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/cortexa9hf-vfp-neon-mx6-pokysdk-linux -V >&5

i686-pokysdk-linux-gcc: error: unrecognized command line option '-V'

i686-pokysdk-linux-gcc: fatal error: no input files

compilation terminated.

configure:3475: $? = 1

configure:3464: i686-pokysdk-linux-gcc -march=i686 --sysroot=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/cortexa9hf-vfp-neon-mx6-pokysdk-linux -qversion >&5

i686-pokysdk-linux-gcc: error: unrecognized command line option '-qversion'

i686-pokysdk-linux-gcc: fatal error: no input files

compilation terminated.

configure:3475: $? = 1

configure:3495: checking whether the C compiler works

configure:3517: i686-pokysdk-linux-gcc -march=i686 --sysroot=/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/cortexa9hf-vfp-neon-mx6-pokysdk-linux -isystem/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/cortexa9hf-vfp-neon-mx6-pokysdk-linux/opt/poky/1.6+snapshot/sysroots/i686-pokysdk-linux/usr/include -O2 -pipe -D_GNU_SOURCE -isystem/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/cortexa9hf-vfp-neon-mx6-pokysdk-linux/opt/poky/1.6+snapshot/sysroots/i686-pokysdk-linux/usr/include -L/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/cortexa9hf-vfp-neon-mx6-pokysdk-linux/opt/poky/1.6+snapshot/sysroots/i686-pokysdk-linux/usr/lib -Wl,-rpath-link,/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/cortexa9hf-vfp-neon-mx6-pokysdk-linux/opt/poky/1.6+snapshot/sysroots/i686-pokysdk-linux/usr/lib -Wl,-rpath,/opt/poky/1.6+snapshot/sysroots/i686-pokysdk-linux/usr/lib -Wl,-O1 -L/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/cortexa9hf-vfp-neon-mx6-pokysdk-linux/opt/poky/1.6+snapshot/sysroots/i686-pokysdk-linux/lib -Wl,-rpath-link,/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/cortexa9hf-vfp-neon-mx6-pokysdk-linux/opt/poky/1.6+snapshot/sysroots/i686-pokysdk-linux/lib -Wl,-rpath,/opt/poky/1.6+snapshot/sysroots/i686-pokysdk-linux/lib -Wl,-O1 conftest.c  >&5

/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find crt1.o: No such file or directory

/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find crti.o: No such file or directory

/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find crtbegin.o: No such file or directory

/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find -lgcc

/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find -lgcc_s

/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find -lc

/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find -lgcc

/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find -lgcc_s

/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find crtend.o: No such file or directory

/home/opti/sandbox/mahyar-ym/build/tmp/sysroots/x86_64-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find crtn.o: No such file or directory

collect2: error: ld returned 1 exit status

configure:3521: $? = 1

configure:3559: result: no

configure: failed program was:

| /* confdefs.h */

| #define PACKAGE_NAME ""

| #define PACKAGE_TARNAME ""

| #define PACKAGE_VERSION ""

| #define PACKAGE_STRING ""

| #define PACKAGE_BUGREPORT ""

| #define PACKAGE_URL ""

| #define PACKAGE "alsa-lib"

| #define VERSION "1.0.27.2"

| /* end confdefs.h.  */

|

| int

| main ()

| {

|

|   ;

|   return 0;

| }

configure:3564: error: in `/home/opti/sandbox/mahyar-ym/build/tmp/work/cortexa9hf-vfp-neon-mx6-pokysdk-linux/nativesdk-alsa-lib/1.0.27.2-r0/build':

configure:3566: error: C compiler cannot create executables

Original Attachment has been moved to: local.conf.zip

Original Attachment has been moved to: bblayers.conf.zip

14 Replies

5,114 Views
aurelienbouin
Contributor IV

Hello,

I do have exactly the same problem, using ubuntu 14.04 with freescale yocto master

The same fail when nativesdk-alsa-lib is configuring ...

When i look into the config.log I also see :

tmp/sysroots/i686-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find crt1.o: No such file or directory

tmp/sysroots/i686-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find crti.o: No such file or directory

tmp/sysroots/i686-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find crtbegin.o: No such file or directory

tmp/sysroots/i686-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find -lgcc

tmp/sysroots/i686-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find -lgcc_s

tmp/sysroots/i686-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find -lc

tmp/sysroots/i686-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find -lgcc

tmp/sysroots/i686-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find -lgcc_s

tmp/sysroots/i686-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find crtend.o: No such file or directory

tmp/sysroots/i686-linux/usr/libexec/i686-pokysdk-linux/gcc/i686-pokysdk-linux/4.9.1/ld: cannot find crtn.o: No such file or directory

collect2: error: ld returned 1 exit status

I am wondering if it is normal that it compiles nativesdk-alsa-lib into tmp/work/cortexa9hf-vfp-neon-mx6-pokysdk-linux/ ?

Thank you ...

0 Kudos
Reply

5,114 Views
gauthier
Contributor III

I have the same issue

| checking for x86_64-pokysdk-linux-gcc... x86_64-pokysdk-linux-gcc  --sysroot=/home/gauthier/numpy-fsl-community-bsp/build/tmp/sysroots/cortexa9hf-vfp-neon-mx6-pokysdk-linux

| checking whether the C compiler works... no

| configure: error: in `/home/gauthier/numpy-fsl-community-bsp/build/tmp/work/cortexa9hf-vfp-neon-mx6-pokysdk-linux/nativesdk-alsa-lib/1.0.27.2-r0/build':

| configure: error: C compiler cannot create executables

1. it is looking for a x86_64 compiler, while I am targeting an i.MX6.

2. the sysroot argument looks at cortexa9hf-vfp-neon-mx6-pokysdk-linux while for my target it should be imx6qsabresd (I think. That's where the images are usually placed.)

At the top of the log, I see this:

| DEBUG: Executing python function sysroot_cleansstate

| DEBUG: Python function sysroot_cleansstate finished

| DEBUG: SITE files ['endian-little', 'common-linux', 'common-glibc', 'bit-64', 'x86_64-linux', 'common']

and this:

| NOTE: Executing ACLOCAL="aclocal --system-acdir=/home/gauthier/numpy-fsl-community-bsp/build/tmp/work/cortexa9hf-vfp-neon-mx6-pokysdk-linux/nativesdk-alsa-lib/1.0.27.2-r0/build/aclocal-copy/" autoreconf --verbose --install --force --exclude=autopoint -I /home/gauthier/numpy-fsl-community-bsp/build/tmp/work/cortexa9hf-vfp-neon-mx6-pokysdk-linux/nativesdk-alsa-lib/1.0.27.2-r0/alsa-lib-1.0.27.2/m4/ -I /home/gauthier/numpy-fsl-community-bsp/build/tmp/work/cortexa9hf-vfp-neon-mx6-pokysdk-linux/nativesdk-alsa-lib/1.0.27.2-r0/alsa-lib-1.0.27.2/utils/

Isn't is a little strange that it is trying to work in cortexa9hf, when my images usually get stored in imx6sabresd?

0 Kudos
Reply

5,114 Views
OtavioSalvador
Senior Contributor II

Hello,

I fixed this in master and daisy branches. Please do 'repo sync' and try again.    

5,110 Views
bryan_prather
Contributor II

Otavio,

Thanks for fixing the compile issue with alsa.  Your changes worked and got me past the original problem.  However, there are two other issues that exist with the configuration I am using (this may need to be put in a separate thread).

The following is the process I followed and the repostories where I got the files (see attached file "build-28Aug14" for details).

cd sandbox

mkdir mahyar-ym

cd mahyar-ym

curl https://storage.googleapis.com/git-repo-downloads/repo > repo

chmod a+x repo

Get Freescale

./repo init -u https://github.com/Freescale/fsl-community-bsp-platform -b master

./repo sync

cd sources

Get meta-boundary

git clone -b master https://github.com/mahyar-ym/meta-boundary.git

Get meta-qt5

git clone -b master https://github.com/meta-qt5/meta-qt5.git

Remove browser from Boundary devices

cd meta-boundary

rm -rf recipes-browser

cd ../..

Removed the following from meta-fsl-arm (don't know if this is necessary but saw it in the post "Qt 5.3.0 release on i.MX6 using fsl-community-bsp and meta-qt5"):

meta-fsl-arm/qt5-layer/recipes-qt/qt5/qtmultimedia_%.bbappend

Initialize environment

MACHINE=nitrogen6x . setup-environment build

Add the following to the end of BBLAYERS in bblayers.conf

${BSPDIR}/sources/meta-qt5 \

${BSPDIR}/sources/meta-boundary \

Edit local.conf

See attached “local.conf”.

Build Tool chain

bitbake meta-toolchain-qt5

It will fail the first time on the multimedia gsttools.

Manually applied the changes from the attached file "multimedia.patch" which came from the following site.

://build.tizen.org/package/view_file?expand=1&file=_service%3Agbs%3A0002-Fix-compilation-when-buildi...

bitbake meta-toolchain-qt5

failed due to PACKAGE_ARCH error - see attached build log.

Had to do: bitbake -c cleanall meta-toolchain-qt5

bitbake meta-toolchain-qt5

tool chain was built successfully.

Build Image

bitbake core-image-minimal

failed due to PACKAGE_ARCH error - see attached build log.

Had to do: bitbake -c cleanall meta-toolchain-qt5

bitbake core-image-minimal

image was built successfully

0 Kudos
Reply

5,110 Views
lutzaltmann
Contributor I

Works! - thanks a lot!

0 Kudos
Reply

5,110 Views
gauthier
Contributor III

Tested, working (daisy).

Thanks, you rock!

0 Kudos
Reply

5,110 Views
jamesbone
NXP TechSupport
NXP TechSupport

Have you try to post your question on SabreLite Community, from Boundary Devices?.   

0 Kudos
Reply

5,110 Views
EricNelson
Senior Contributor II

Hi James,

Bryan has reached out to us, and we haven't had a chance to try and reproduce this (we're hardly Yocto experts).

My best guess here is that the problem stems from an order-of-events thing.

As I understand it, before building the toolchain (meta-toolchain-qt5), you first need to build an image with the run-time components, so that the toolchain build knows which headers, libraries, and such to include in the development environment.

bryan.prather@optimedical.com, did you build the run-time image successfully first? Your local.conf seems to include the "dev-pkgs" feature (I think that's needed).

0 Kudos
Reply

5,110 Views
bryan_prather
Contributor II

I did build the core-image-minimal before building the tool chain.

0 Kudos
Reply

5,110 Views
OtavioSalvador
Senior Contributor II

Hello bryan.prather@optimedical.com

One thing I noticed from your platform description is that you are using master. We had some hard time in master these days and we're still recovering from it ;-)

The meta-toolchain-qt5 ought to be self-contained so you don't need to build any recipe before building it.

So now back to the topic, it seems you have a broken sysroot as the core libraries from GCC and GlibC are missing.

In this situation the easiest is to start over; so remove your tmp directory and start a new plain build. If it still fails, drop the sstate-cache and tmp directory. In stable branches this is very rare to be necessary as metadata is stable but in master those surprises happen from time to time.

0 Kudos
Reply

5,110 Views
bryan_prather
Contributor II

Otavio - thanks for your response.

What branch should I use if not master?

I did remove the tmp directory and everything in the build directory except for the conf directory.  The problem still exists.

0 Kudos
Reply

5,110 Views
OtavioSalvador
Senior Contributor II

daisy branch.

I have customers using Qt5 in daisy with no issues.

0 Kudos
Reply

5,109 Views
bryan_prather
Contributor II

I deleted everything and got the boundary devices master branch from (no daisy branch available) https://github.com/mahyar-ym/boundary-community-bsp-base.  I deleted the meta-qt5 in the sources directory and replaced it with the daisy branch as follows (I don't know if this is valid):

"git clone -b daisy https://github.com/meta-qt5/meta-qt5.git.

I built the meta-toolchain-qt5 and got the same error (see attached).

I'm using Ubuntu 12.04.  Should I upgrade to 14.04?

0 Kudos
Reply

5,108 Views
lutzaltmann
Contributor I

Hello!

I think i've the same or problem.

i'm using ubuntu 14.04. and try to bitbake the "meta-toolchain" for nitrogen6x.

The configure of the alsa lib fails: "nativesdk-alsa-lib-1.0.27.2-r0 do_configure"

I've attached the logfile!

Error:

checking for x86_64-pokysdk-linux-gcc... x86_64-pokysdk-linux-gcc  --sysroot=/iosono/imx6/yocto/master-next/build/tmp/sysroots/cortexa9hf-vfp-neon-mx6-pokysdk-linux

checking whether the C compiler works... no

Maybe the problem is related to the given sysroot path - because the given path doesn't exist on my machine

- maybe this is the problem?

I appreciate every hint you might have.

regards,

Lutz Altmann