Configure both csi0 and csi1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Configure both csi0 and csi1

923 次查看
dengguozhen
Contributor I

In imx8qm, csi0 and csi1 need to be used at the same time. In addition to being configured in DTS, is it necessary to configure elsewhere? I set the status attribute in the nodes of csi0 and csi1 to okay, but only csi0 is loaded

0 项奖励
回复
1 回复

862 次查看
igorpadykov
NXP Employee
NXP Employee

Hi guozhen

yes they can be used in the same time, one can try

with fsl-imx8qm-mek-mipi-two-ov5640.dts:

fsl-imx8qm-mek-mipi-two-ov5640.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复