RPMsg-lite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RPMsg-lite

3,354 Views
savithaunni26
Contributor I

Hi, 

My question is about RPMsg-lite. I need to build a user App which can demonstrate the use of RPMsg-lite.Something like a wrapper over the RPMsg-lite.Do we have examples for this to understand it a little better?

Thanks

Tags (1)
0 Kudos
Reply
2 Replies

3,056 Views
igorpadykov
NXP Employee
NXP Employee

Hi Savitha

"officially" supported software is described on (seems there is no (RPMsg-lite)

i.MX Software | NXP 

One can look on

RPMsg-Lite User's Guide: RPMsg Component 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,055 Views
savithaunni26
Contributor I

Thanks Igor!

0 Kudos
Reply