Configure both csi0 and csi1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configure both csi0 and csi1

1,309件の閲覧回数
dengguozhen
Contributor I

In imx8qm, csi0 and csi1 need to be used at the same time. In addition to being configured in DTS, is it necessary to configure elsewhere? I set the status attribute in the nodes of csi0 and csi1 to okay, but only csi0 is loaded

0 件の賞賛
返信
1 返信

1,248件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi guozhen

yes they can be used in the same time, one can try

with fsl-imx8qm-mek-mipi-two-ov5640.dts:

fsl-imx8qm-mek-mipi-two-ov5640.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信