Configure and usage of OCRAM for load and run the firmware of M core from imx93 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configure and usage of OCRAM for load and run the firmware of M core from imx93 board

201 Views
rk4
Contributor I

Hi NXP Team, 

 

Can you explain me exact procedure to use the OCRAM for load and run the firmware (elf file) by remoteproc on M33 core of imx93 board (Digi core connect93).

 

I want OCRAM because the TCM memory has only 128KB available for data and text sections both and I cannot exceed it to 256KB.

 

I want the complete procedure from A core as well M core side to configure OCRAM and run the code larger than the 128KB for our application purpose.

 

Please help me in here. Please ask me if you have any questions regarding this.

 

Thanks

0 Kudos
Reply
0 Replies