Config Tool Update causes DDR error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Config Tool Update causes DDR error

ソリューションへジャンプ
4,101件の閲覧回数
lcotten
Contributor II

I've updated the Config Tools for i.MX to Version 13.1. The updated DDR tool now has a constant error "Failed to generate code" (see picture). Its says "tool problem" and offers no specific issue. Even when I create a new from scratch configuration, the same thing happens. If I change any setting, I get a 'not supported"  error. The CPU selected is MIMX8ML4xxxKZ. The Pin tools still works fine as far as I can tell. To reproduce, open the new, create a new config, select MIMX8ML4xxxKZ. Go back and forth between pin tool and DDR tool a couple of times and/or do an "Update Code".

ToolProblem.pngToolProblem.png

ラベル(1)
0 件の賞賛
返信
1 解決策
4,076件の閲覧回数
lcotten
Contributor II

I tried that. It didn't work. So, I uninstalled the app, deleted the whole "mcu_data_v13" folder (kept a copy), and reinstalled. Then I created a new config, and the problem is fixed. I was then able to import all my pin settings. So, I think all is well now. One interesting note: even after a fresh reinstallation, when I create new configs, the DDR tool comes up with my swizzle already in it. 

 

Is there yet another badge for this? (kidding!)

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,077件の閲覧回数
lcotten
Contributor II

I tried that. It didn't work. So, I uninstalled the app, deleted the whole "mcu_data_v13" folder (kept a copy), and reinstalled. Then I created a new config, and the problem is fixed. I was then able to import all my pin settings. So, I think all is well now. One interesting note: even after a fresh reinstallation, when I create new configs, the DDR tool comes up with my swizzle already in it. 

 

Is there yet another badge for this? (kidding!)

0 件の賞賛
返信
4,065件の閲覧回数
addiyi
NXP Employee
NXP Employee

You can check the Preset. If it is Custom then changes are applied to default configuration, otherwise it should show Default LPDDR4 Configuration.

 

addiyi_0-1683286698723.pngaddiyi_0-1683286698723.png

 

0 件の賞賛
返信
4,085件の閲覧回数
addiyi
NXP Employee
NXP Employee

Please go to C:\ProgramData\NXP\mcu_data_v13 and delete the processor folder. After that recreate the project from scratch.

Adrian

0 件の賞賛
返信