Compressive load result to the package in i.MX6SLX .

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Compressive load result to the package in i.MX6SLX .

跳至解决方案
926 次查看
takashitakahash
Contributor III

Hi community.

Our customer has question below.

Would you Please indicate the pressure Measurement results or simulation results to determine that on the practical use

when added compression load to 100 N (10 kg), 300N (30 kg), 1000 N (100 kg) at the i.MX6SLX BGA package.

(Verify the presence or absence of stress to the internal circuit of IMX6SLX.

标签 (1)
0 项奖励
回复
1 解答
859 次查看
art
NXP Employee
NXP Employee

All typical packages of the i.MX series processors are rated for 10lbs (approx. 4.5kg) of constant additional surface pressure.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
860 次查看
art
NXP Employee
NXP Employee

All typical packages of the i.MX series processors are rated for 10lbs (approx. 4.5kg) of constant additional surface pressure.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复