Compressive load result to the package in i.MX6SLX .

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compressive load result to the package in i.MX6SLX .

ソリューションへジャンプ
954件の閲覧回数
takashitakahash
Contributor III

Hi community.

Our customer has question below.

Would you Please indicate the pressure Measurement results or simulation results to determine that on the practical use

when added compression load to 100 N (10 kg), 300N (30 kg), 1000 N (100 kg) at the i.MX6SLX BGA package.

(Verify the presence or absence of stress to the internal circuit of IMX6SLX.

ラベル(1)
0 件の賞賛
返信
1 解決策
887件の閲覧回数
art
NXP Employee
NXP Employee

All typical packages of the i.MX series processors are rated for 10lbs (approx. 4.5kg) of constant additional surface pressure.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
888件の閲覧回数
art
NXP Employee
NXP Employee

All typical packages of the i.MX series processors are rated for 10lbs (approx. 4.5kg) of constant additional surface pressure.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信