Compressive load result to the package in i.MX6SLX .

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compressive load result to the package in i.MX6SLX .

Jump to solution
951 Views
takashitakahash
Contributor III

Hi community.

Our customer has question below.

Would you Please indicate the pressure Measurement results or simulation results to determine that on the practical use

when added compression load to 100 N (10 kg), 300N (30 kg), 1000 N (100 kg) at the i.MX6SLX BGA package.

(Verify the presence or absence of stress to the internal circuit of IMX6SLX.

Labels (1)
0 Kudos
Reply
1 Solution
884 Views
art
NXP Employee
NXP Employee

All typical packages of the i.MX series processors are rated for 10lbs (approx. 4.5kg) of constant additional surface pressure.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
885 Views
art
NXP Employee
NXP Employee

All typical packages of the i.MX series processors are rated for 10lbs (approx. 4.5kg) of constant additional surface pressure.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply