Compiling Kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Compiling Kernel

跳至解决方案
2,093 次查看
Ketki
Contributor I

I was using Android 7.1 with EDM1-iMX6 Dual Lite board with Fairy as baseboard.
On using flashcard script to flash the code boot partition was created with zImage in Android 7.1.
We would make changes to the kernel with make menuconfig and fire the command make zImage to update the build and the changes were reflected.
Now I am switching to Android 9.0 with EDM1-iMX6Q board with Fairy as baseboard.
On using the same script the partitions are different and there is no boot folder or I cannot see any zImage in the folder. 
I make changes to the kernel with make menuconfig but make zImage does not reflect the same.
What command do I use instead on make zImage to update my changes from make menuconfig ?

 

0 项奖励
回复
1 解答
2,080 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Ketki,

Is possible that you run the script instead of kernel image then you have the virtual kernel partition overwrites only the kernel (zImage, zImage-dtb, Image.gz-dtb) by writing the new image.

But you need the Zimage you have to git clone https://source.codeaurora.org/external/imx/linux-imx and menuconfig and make your configuration and build.

You may ask  to EDM1-iMX6 manufacturer if they changed the script.

Regards

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,081 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Ketki,

Is possible that you run the script instead of kernel image then you have the virtual kernel partition overwrites only the kernel (zImage, zImage-dtb, Image.gz-dtb) by writing the new image.

But you need the Zimage you have to git clone https://source.codeaurora.org/external/imx/linux-imx and menuconfig and make your configuration and build.

You may ask  to EDM1-iMX6 manufacturer if they changed the script.

Regards

 

0 项奖励
回复