USB Vbus drop in OTG mode on iMX8QM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Vbus drop in OTG mode on iMX8QM

Jump to solution
1,328 Views
fmonte
Contributor IV

Hello,

on iMX8Qm when I set the USB port to OTG mode (by setting the USB_OTG2_ID pad) the power enable pad (SS3_TC0) voltage drops, causing in a drop of the Vbus on the OTG port.

This is actually correct by reading the OTG specification. However, is it possible to control the SS3_TC0/USB_OTG1_PWR signal, regardless of the OTG/host status?

 

Thank you!

Francesco

0 Kudos
Reply
1 Solution
1,305 Views
igorpadykov
NXP Employee
NXP Employee

Hi Francesco

 

>Is it possible to keep the Vbus in OTG mode by reconfiguring some register?

 

not.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
3 Replies
1,319 Views
igorpadykov
NXP Employee
NXP Employee

Hi Francesco

 

seems one can reconfigure SS3_TC0 as GPIO4_IO03 and make

necessary modifications in driver.

 

Best regards
igor

0 Kudos
Reply
1,314 Views
fmonte
Contributor IV

Hi Igor,

I know that muxing to GPIO is a possible solution. However, we cannot do that since in SCU FW port the GPIO4 device is assigned to a reserved HW partition.

Is it possible to keep the Vbus in OTG mode by reconfiguring some register?

0 Kudos
Reply
1,306 Views
igorpadykov
NXP Employee
NXP Employee

Hi Francesco

 

>Is it possible to keep the Vbus in OTG mode by reconfiguring some register?

 

not.

 

Best regards
igor

0 Kudos
Reply