Compiler problem with KSZ8895

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compiler problem with KSZ8895

3,161 Views
emintolgasivri
Contributor II

I am using IMX7dea Ucom Som board and Ksz8895 ethernet switch chip.I used SPI interface between mpu and ethernet chip.I add linux driver to mey kernel but i didnt see xx.o file.I guss ccross compile didnt worked.Ant it didnt creat xx.o files.I used KSZ8895 Linux driver for revision 3.3 tared.

How can I fix this?

Also I saw writing blove these in KSZ8895MQ/RQ Evaluation Board User’s Guide

The KSZ8895 will power up initial default configuration with the start switch in register 1 bit 0
= ‘0’ which means the switch is “off”. You can set the bit 0 =’1’ to start switch.

How Can I change this register with spi interface?

Thanks.

Labels (3)
Tags (2)
0 Kudos
Reply
1 Reply

3,012 Views
igorpadykov
NXP Employee
NXP Employee

Hi Emin

one can look at Yocto project documentation

Adding the WF111 Driver to the i.MX6 Yocto BSP 

https://community.nxp.com/thread/444387 

i.MX Yocto Project: How can I (quickly) modify the kernel and test it? 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply