Compiler problem with KSZ8895

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compiler problem with KSZ8895

2,289件の閲覧回数
emintolgasivri
Contributor II

I am using IMX7dea Ucom Som board and Ksz8895 ethernet switch chip.I used SPI interface between mpu and ethernet chip.I add linux driver to mey kernel but i didnt see xx.o file.I guss ccross compile didnt worked.Ant it didnt creat xx.o files.I used KSZ8895 Linux driver for revision 3.3 tared.

How can I fix this?

Also I saw writing blove these in KSZ8895MQ/RQ Evaluation Board User’s Guide

The KSZ8895 will power up initial default configuration with the start switch in register 1 bit 0
= ‘0’ which means the switch is “off”. You can set the bit 0 =’1’ to start switch.

How Can I change this register with spi interface?

Thanks.

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 返信

2,140件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Emin

one can look at Yocto project documentation

Adding the WF111 Driver to the i.MX6 Yocto BSP 

https://community.nxp.com/thread/444387 

i.MX Yocto Project: How can I (quickly) modify the kernel and test it? 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信