Codeaurora sources migrated

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codeaurora sources migrated

5,530件の閲覧回数
BHAVANI_S
Contributor I

Hi All,

It is come to the notice that the sources of imx that were present in the codeaurora site has been closed and the repositories have been moved to the NXP github.

Please let us know the alternative sources for the below mentioned repos in code aurora and the permission required to download them. We are having a high priority release and are blocked because of this.

"https://source.codeaurora.org/external/imx/aosp/"

"https://source.codeaurora.org/external/imx/android-imx

"https://source.codeaurora.org/external/imx/

Thanks and Regards,

Bhavani S

 

0 件の賞賛
返信
4 返答(返信)

5,426件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

i.mx page at nxp-imx · GitHub and can get updates from release note i.MX Linux Release Notes (nxp.com)

 

Best regards

Harvey

0 件の賞賛
返信

3,756件の閲覧回数
yeswanth
Contributor II

i can't find for the following repositories in github they have similar names, could you mention the exact repositories in github for the following:

name="android-imx"
fetch="https://source.codeaurora.org/external/imx/aosp/"

name="android-imx-orig"
fetch="https://source.codeaurora.org/external/imx/android-imx"

0 件の賞賛
返信

5,506件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

You can find all the Android repositories here:

https://github.com/nxp-imx-android

Regards,

Gary

0 件の賞賛
返信

2,698件の閲覧回数
pholden
Contributor III

I have to build the kirkstone branch of Qoriq Yocto for a client.  I'm getting the following error:

 

eth-config-git-r2 do_fetch: Fetcher failure

 

It's pointing to codeaurora.org.  Where did this package move to?

 

Thanks!

タグ(2)
0 件の賞賛
返信