Codeaurora sources migrated

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Codeaurora sources migrated

3,652 次查看
BHAVANI_S
Contributor I

Hi All,

It is come to the notice that the sources of imx that were present in the codeaurora site has been closed and the repositories have been moved to the NXP github.

Please let us know the alternative sources for the below mentioned repos in code aurora and the permission required to download them. We are having a high priority release and are blocked because of this.

"https://source.codeaurora.org/external/imx/aosp/"

"https://source.codeaurora.org/external/imx/android-imx

"https://source.codeaurora.org/external/imx/

Thanks and Regards,

Bhavani S

 

0 项奖励
回复
4 回复数

3,548 次查看
Harvey021
NXP TechSupport
NXP TechSupport

i.mx page at nxp-imx · GitHub and can get updates from release note i.MX Linux Release Notes (nxp.com)

 

Best regards

Harvey

0 项奖励
回复

1,878 次查看
yeswanth
Contributor II

i can't find for the following repositories in github they have similar names, could you mention the exact repositories in github for the following:

name="android-imx"
fetch="https://source.codeaurora.org/external/imx/aosp/"

name="android-imx-orig"
fetch="https://source.codeaurora.org/external/imx/android-imx"

0 项奖励
回复

3,628 次查看
gary_bisson
Senior Contributor III

Hi,

You can find all the Android repositories here:

https://github.com/nxp-imx-android

Regards,

Gary

0 项奖励
回复

820 次查看
pholden
Contributor III

I have to build the kirkstone branch of Qoriq Yocto for a client.  I'm getting the following error:

 

eth-config-git-r2 do_fetch: Fetcher failure

 

It's pointing to codeaurora.org.  Where did this package move to?

 

Thanks!

标记 (2)
0 项奖励
回复