Code Signing Tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Code Signing Tool

跳至解决方案
3,911 次查看
friederbaumgrat
Contributor III

Dear NXP community,

I have a question. Is it possible to tell the Code Signing Tool to use a specific key to encrypt an image?

Regards,

Frieder

标签 (1)
0 项奖励
回复
1 解答
3,508 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  The Code Signing Tool automatically generates a random DEK, if the “Install Secret Key”
command is present in the CSF and CST is in encryption mode. No ability to use a specific

key instead of automatically generated one.

Regards,

Yuri.

在原帖中查看解决方案

3 回复数
3,508 次查看
brianmiller
Contributor II

The CST back-end source code contains code to read a pre-existing DEK key.  To use it, you'll need to modify the back-end code.

3,509 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  The Code Signing Tool automatically generates a random DEK, if the “Install Secret Key”
command is present in the CSF and CST is in encryption mode. No ability to use a specific

key instead of automatically generated one.

Regards,

Yuri.

3,508 次查看
friederbaumgrat
Contributor III

Dear Yuri,

thanks for your answer.

Best Regards,

Frieder

0 项奖励
回复