Code Signing Tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Signing Tool

Jump to solution
4,081 Views
friederbaumgrat
Contributor III

Dear NXP community,

I have a question. Is it possible to tell the Code Signing Tool to use a specific key to encrypt an image?

Regards,

Frieder

Labels (1)
0 Kudos
Reply
1 Solution
3,678 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The Code Signing Tool automatically generates a random DEK, if the “Install Secret Key”
command is present in the CSF and CST is in encryption mode. No ability to use a specific

key instead of automatically generated one.

Regards,

Yuri.

View solution in original post

3 Replies
3,678 Views
brianmiller
Contributor II

The CST back-end source code contains code to read a pre-existing DEK key.  To use it, you'll need to modify the back-end code.

3,678 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The Code Signing Tool automatically generates a random DEK, if the “Install Secret Key”
command is present in the CSF and CST is in encryption mode. No ability to use a specific

key instead of automatically generated one.

Regards,

Yuri.

3,678 Views
friederbaumgrat
Contributor III

Dear Yuri,

thanks for your answer.

Best Regards,

Frieder

0 Kudos
Reply