Code Signing Tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,903件の閲覧回数
friederbaumgrat
Contributor III

Dear NXP community,

I have a question. Is it possible to tell the Code Signing Tool to use a specific key to encrypt an image?

Regards,

Frieder

ラベル(1)
0 件の賞賛
返信
1 解決策
3,500件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The Code Signing Tool automatically generates a random DEK, if the “Install Secret Key”
command is present in the CSF and CST is in encryption mode. No ability to use a specific

key instead of automatically generated one.

Regards,

Yuri.

元の投稿で解決策を見る

3 返答(返信)
3,500件の閲覧回数
brianmiller
Contributor II

The CST back-end source code contains code to read a pre-existing DEK key.  To use it, you'll need to modify the back-end code.

3,501件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The Code Signing Tool automatically generates a random DEK, if the “Install Secret Key”
command is present in the CSF and CST is in encryption mode. No ability to use a specific

key instead of automatically generated one.

Regards,

Yuri.

3,500件の閲覧回数
friederbaumgrat
Contributor III

Dear Yuri,

thanks for your answer.

Best Regards,

Frieder

0 件の賞賛
返信