Clutter based app failed to initialize

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clutter based app failed to initialize

2,069件の閲覧回数
nkt
Contributor I

I am using iMX6 sabreauto dual lite. I am trying to create application based on clutter with x11 and mesa is my rendering component (not using hw rendering). When I execute example application, below error is shown.

May I know the reason for this error and also solution?

~# ./basic-actor
[     1] HAL user version 5.0.11 build 41671
[     2] HAL kernel version 5.0.11 build 33433
[     3] HAL user version 5.0.11 build 41671
[     4] HAL kernel version 5.0.11 build 33433
[     5] HAL user version 5.0.11 build 41671
[     6] HAL kernel version 5.0.11 build 33433
[     7] HAL user version 5.0.11 build 41671
[     8] HAL kernel version 5.0.11 build 33433

(basic-actor:235): Clutter-CRITICAL **: Unable to initialize Clutter: Failed to connected to any renderer due to constraints

Appreciate your help.

Regards,

NKT

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,861件の閲覧回数
nkt
Contributor I

Jimmychan, I saw bbappend file. it uses CFLAGS_append_mx6 and PACKAGECONFIG_mx6?

is mx6 variant applicable for iMX6 sabreauto dual lite? 

0 件の賞賛
返信

1,861件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信