Clutter based app failed to initialize

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clutter based app failed to initialize

2,074 Views
nkt
Contributor I

I am using iMX6 sabreauto dual lite. I am trying to create application based on clutter with x11 and mesa is my rendering component (not using hw rendering). When I execute example application, below error is shown.

May I know the reason for this error and also solution?

~# ./basic-actor
[     1] HAL user version 5.0.11 build 41671
[     2] HAL kernel version 5.0.11 build 33433
[     3] HAL user version 5.0.11 build 41671
[     4] HAL kernel version 5.0.11 build 33433
[     5] HAL user version 5.0.11 build 41671
[     6] HAL kernel version 5.0.11 build 33433
[     7] HAL user version 5.0.11 build 41671
[     8] HAL kernel version 5.0.11 build 33433

(basic-actor:235): Clutter-CRITICAL **: Unable to initialize Clutter: Failed to connected to any renderer due to constraints

Appreciate your help.

Regards,

NKT

Labels (1)
0 Kudos
Reply
2 Replies

1,866 Views
nkt
Contributor I

Jimmychan, I saw bbappend file. it uses CFLAGS_append_mx6 and PACKAGECONFIG_mx6?

is mx6 variant applicable for iMX6 sabreauto dual lite? 

0 Kudos
Reply

1,866 Views
jimmychan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply