Changing IPU Parameters via Gstreamer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changing IPU Parameters via Gstreamer

ソリューションへジャンプ
1,837件の閲覧回数
jeromehaxhiaj
Contributor I

Hi everyone,

I'm playing a video with gstreamer on an IMX6 Quad. Is it possible with gstreamer to  select the component which make the CSC ( IC or DP ) ?

Thanks

ラベル(4)
1 解決策
1,654件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jerome

as mentioned on below links option with IC is only available

https://community.freescale.com/thread/308426

https://community.freescale.com/docs/DOC-94961

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,655件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jerome

as mentioned on below links option with IC is only available

https://community.freescale.com/thread/308426

https://community.freescale.com/docs/DOC-94961

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------