Change Screen Resolution Dynamically in WEC7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Change Screen Resolution Dynamically in WEC7

ソリューションへジャンプ
3,516件の閲覧回数
akhil
Contributor III

Currently we are using a HVGA display with resolution 320x480. Is there any method to change the screen resolution dynamically (without reboot)? Is there any driver support for this in Wince 7? The processor used is imx53/imx6.

ラベル(4)
1 解決策
2,983件の閲覧回数
justin_jiang
NXP Employee
NXP Employee

Hi Akhil,

It depends on how many resolution your panel can support.

If you pannel only support 320*480, then it can't by change dynamically.

The panel settings is different for diffrent resolution.

B.R

Justin

元の投稿で解決策を見る

4 返答(返信)
2,984件の閲覧回数
justin_jiang
NXP Employee
NXP Employee

Hi Akhil,

It depends on how many resolution your panel can support.

If you pannel only support 320*480, then it can't by change dynamically.

The panel settings is different for diffrent resolution.

B.R

Justin

2,983件の閲覧回数
YixingKong
Senior Contributor IV

Akhil

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,
Yixing

0 件の賞賛
返信
2,983件の閲覧回数
akhil
Contributor III

We still have the issue, as there is no BSP support for dynamic display resolution changing.

0 件の賞賛
返信
2,983件の閲覧回数
YixingKong
Senior Contributor IV

Akhil

I will branch your discussion into an internal group and assign an engineer to work on it.

Regards,

Yixing

0 件の賞賛
返信