Change Screen Resolution Dynamically in WEC7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change Screen Resolution Dynamically in WEC7

Jump to solution
3,533 Views
akhil
Contributor III

Currently we are using a HVGA display with resolution 320x480. Is there any method to change the screen resolution dynamically (without reboot)? Is there any driver support for this in Wince 7? The processor used is imx53/imx6.

Labels (4)
1 Solution
3,000 Views
justin_jiang
NXP Employee
NXP Employee

Hi Akhil,

It depends on how many resolution your panel can support.

If you pannel only support 320*480, then it can't by change dynamically.

The panel settings is different for diffrent resolution.

B.R

Justin

View solution in original post

4 Replies
3,001 Views
justin_jiang
NXP Employee
NXP Employee

Hi Akhil,

It depends on how many resolution your panel can support.

If you pannel only support 320*480, then it can't by change dynamically.

The panel settings is different for diffrent resolution.

B.R

Justin

3,000 Views
YixingKong
Senior Contributor IV

Akhil

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,
Yixing

0 Kudos
Reply
3,000 Views
akhil
Contributor III

We still have the issue, as there is no BSP support for dynamic display resolution changing.

0 Kudos
Reply
3,000 Views
YixingKong
Senior Contributor IV

Akhil

I will branch your discussion into an internal group and assign an engineer to work on it.

Regards,

Yixing

0 Kudos
Reply