Cant read from SD card Android Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cant read from SD card Android Boot

1,851 Views
jonathansmyth
Contributor III

hi guys,

I cant seem to get my android to boot from the sd card...it keeps giving me this error attached i dont know what the path for the sd card is everything i try gives me an error

custom board that runs imx6dl SOC

Any help would be awesome

NAND write: device 0 offset 0x240000, size 0x4cf800

5044224 bytes written: OK

efusA9 # booti Kernel

kernel   @ 10008000 (4801604)

ramdisk  @ 11000000 (237962)

kernel cmdline:

        use uboot command line:

        console=ttymxc3,115200 login_tty=ttymxc3,115200 mtdparts=gpmi-nand:256k(NBoot)ro,768k(UserDef),256k(Refresh)ro,768k(UBoot)ro,256k(UBootEnv)ro,5888K(Kernel)ro,-(TargetFS) root=/dev/mtdblock0 ro

        Using machid 0x136e

Starting kernel ...

Initializing cgroup subsys cpu

Linux version 3.0.35-F+S (jonathan@jonathan-VirtualBox) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #2 SMP PREEMPT Tue May 12 08:03:41 CEST 2015

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: efusA9

Memory policy: ECC disabled, Data cache writealloc

CPU identified as i.MX6DL/SOLO, silicon rev 1.2

PERCPU: Embedded 7 pages/cpu @80ef7000 s5536 r8192 d14944 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 97280

Kernel command line: noinitrd loglevel=7 no_console_suspend console=ttymxc3,115200 login_tty=ttymxc3,115200 mtdparts=gpmi-nand:256k(NBoot)ro,768k(UserDef),256k(Refresh)ro,768k(UBoot)ro,256k(UBootEnv)ro,5888K(Kernel)ro,-(TargetFS) root=/dev/mtdblock0 ro

PID hash table entries: 2048 (order: 1, 8192 bytes)

Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

Memory: 384MB = 384MB total

Memory: 377464k/377464k available, 146824k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    DMA     : 0xfbe00000 - 0xffe00000   (  64 MB)

    vmalloc : 0xa0800000 - 0xf2000000   (1304 MB)

    lowmem  : 0x80000000 - 0xa0000000   ( 512 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .init : 0x80008000 - 0x80043000   ( 236 kB)

      .text : 0x80043000 - 0x8092c804   (9127 kB)

      .data : 0x8092e000 - 0x809c0498   ( 586 kB)

       .bss : 0x809c04bc - 0x80af18b0   (1221 kB)

SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

Preemptible hierarchical RCU implementation.

NR_IRQS:624

MXC GPIO hardware

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

Set periph_clk's parent to pll2_pfd_400M!

arm_max_freq=1GHz

MXC_Early serial console at MMIO 0x21f0000 (options '115200')

bootconsole [ttymxc3] enabled

Console: colour dummy device 80x30

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Initializing cgroup subsys debug

Initializing cgroup subsys cpuacct

Initializing cgroup subsys freezer

CPU: Testing write buffer coherency: ok

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

Brought up 1 CPUs

SMP: Total of 1 processors activated (1581.05 BogoMIPS).

devtmpfs: initialized

print_constraints: dummy:

NET: Registered protocol family 16

print_constraints: vddpu: 725 <--> 1300 mV at 1150 mV fast normal

print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal

print_constraints: vddsoc: 725 <--> 1300 mV at 1150 mV fast normal

print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal

print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal

print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal

hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.

hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.

hw-breakpoint: maximum watchpoint size is 4 bytes.

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32050000, Cache size: 524288 B

bio: create slab <bio-0> at 0

mxs-dma-ext mxs-dma-ext-apbh: initialized

print_constraints: VDDA: 3300 mV

print_constraints: VDDIO: 3300 mV

print_constraints: VDDD: 1500 mV

print_constraints: vmmc: 3300 mV

vgaarb: loaded

SCSI subsystem initialized

spi_imx imx6q-ecspi.0: probed

spi_imx imx6q-ecspi.1: probed

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

Freescale USB OTG Driver loaded, $Revision: 1.55 $

imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed

mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Version 1.0.24.

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

Switching to clocksource mxc_timer1

cfg80211: Calling CRDA to update world regulatory domain

NET: Registered protocol family 2

IP route cache hash table entries: 4096 (order: 2, 16384 bytes)

TCP established hash table entries: 16384 (order: 5, 131072 bytes)

TCP bind hash table entries: 16384 (order: 5, 196608 bytes)

TCP: Hash tables configured (established 16384 bind 16384)

TCP reno registered

UDP hash table entries: 256 (order: 1, 8192 bytes)

UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Static Power Management for Freescale i.MX6

wait mode is enabled for i.MX6

cpaddr = 0 suspend_iram_base=f2900000

PM driver module loaded

iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.

PCIE: imx_pcie_pltfm_probe start link up.

link up failed, DB_R0:0x009b2200, DB_R1:0x08200000!

IMX PCIe port: link down with power supply 0!

IMX usb wakeup probe

add wake up source irq 75

IMX usb wakeup probe

cpu regulator mode:ldo_enable

i.MXC CPU frequency driver

ashmem: initialized

squashfs: version 4.0 (2009/01/31) Phillip Lougher

JFFS2 version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.

ROMFS MTD (C) 2007 Red Hat, Inc.

fuse init (API version 7.16)

msgmni has been set to 737

alg: No test for stdrng (krng)

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb

_regulator_get: get() with no identifier

Console: switching to colour frame buffer device 100x30

mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver lcd

imx-sdma imx-sdma: loaded firmware 1.1

imx-sdma imx-sdma: initialized

Serial: IMX driver

imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX

imx-uart.1: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX

imx-uart.3: ttymxc3 at MMIO 0x21f0000 (irq = 61) is a IMX

console [ttymxc3] enabled, bootconsole disabled

console [ttymxc3] enabled, bootconsole disabled

imx-uart.4: ttymxc4 at MMIO 0x21f4000 (irq = 62) is a IMX

[drm] Initialized drm 1.1.0 20060810

[drm] Initialized vivante 1.0.0 20120216 on minor 0

brd: module loaded

loop: module loaded

at24 0-0057: 2048 byte at24 EEPROM, writable, 8 bytes/write

m25p80 spi0.0: found m25p05-nonjedec, expected sst25vf016b

m25p80 spi0.0: m25p05-nonjedec (64 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x000000000000-0x000000040000 : "bootloader"

mtd: partition "bootloader" extends beyond the end of device "m25p80" -- size truncated to 0x10000

0x000000010000-0x000000010000 : "kernel"

mtd: partition "kernel" is out of reach -- disabled

ONFI flash detected

ONFI param page 0 valid

NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron MT29F2G08ABAEAH4)

gpmi-nand-fus imx6q-gpmi-nand-fus.0: enable asynchronous EDO mode 5

Scanning device for bad blocks

7 cmdlinepart partitions found on MTD device gpmi-nand

Creating 7 MTD partitions on "gpmi-nand":

0x000000000000-0x000000040000 : "NBoot"

0x000000040000-0x000000100000 : "UserDef"

0x000000100000-0x000000140000 : "Refresh"

0x000000140000-0x000000200000 : "UBoot"

0x000000200000-0x000000240000 : "UBootEnv"

0x000000240000-0x000000800000 : "Kernel"

0x000000800000-0x000010000000 : "TargetFS"

GPMI NAND driver registered. (IMX)

vcan: Virtual CAN interface driver

CAN device driver interface

flexcan netdevice driver

flexcan imx6q-flexcan.0: device registered (reg_base=a09b0000, irq=142)

flexcan imx6q-flexcan.1: device registered (reg_base=a09b8000, irq=143)

FEC Ethernet Driver

fec_enet_mii_bus: probed

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000

fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

add wake up source irq 72

fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2

fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200

fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

ARC USBOTG Device Controller driver (1 August 2005)

android_usb gadget: Mass Storage Function, version: 2009/09/11

android_usb gadget: Number of LUNs=1

lun0: LUN: removable file: (no medium)

Gadget Android: controller 'fsl-usb2-udc' not recognized

android_usb gadget: android_usb ready

Suspend udc for OTG auto detect

fsl-usb2-udc: bind to driver android_usb

mousedev: PS/2 mouse device common for all mice

input: gpio-keys as /devices/platform/gpio-keys/input/input0

atmel_mxt_ts 1-004a: __mxt_read_reg: i2c transfer failed (-5)

atmel_mxt_ts: probe of 1-004a failed with error -5

sx8655 1-0049: sx8655_probe()

sx8655 1-0049: write mask fail

sx8655: probe of 1-0049 failed with error -5

rtc-pcf8563 0-0051: chip found, driver version 0.4.3

rtc-pcf8563 0-0051: low voltage detected, date/time is not reliable.

using rtc device, rtc-pcf8563, for alarms

rtc-pcf8563 0-0051: rtc core: registered rtc-pcf8563 as rtc0

i2c /dev entries driver

Linux video capture interface: v2.00

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18

imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)

Bluetooth: HCI UART driver ver 2.2

Bluetooth: HCI H4 protocol initialized

Bluetooth: HCI BCSP protocol initialized

Bluetooth: HCILL protocol initialized

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci sdhci-esdhc-imx.2: no write-protect pin available!

sdhci sdhci-esdhc-imx.2: no card-detect pin available!

android_work: did not send uevent (0 0   (null))

mmc0: SDHCI controller on platform [sdhci-esdhc-imx.2] using ADMA

mmc1: SDHCI controller on platform [sdhci-esdhc-imx.1] using ADMA

mmc2: SDHCI controller on platform [sdhci-esdhc-imx.0] using ADMA

mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

VPU initialized

mxc_asrc registered

Galcore version 4.6.9.9754

android_work: sent uevent USB_STATE=CONNECTED

android_work: sent uevent USB_STATE=DISCONNECTED

revserved_memory_account:viv_gpu registerd

Thermal calibration data is 0x58e4ec69

Thermal sensor with ratio = 184

Anatop Thermal registered as thermal_zone0

anatop_thermal_probe: default cooling device is cpufreq!

usb 2-1: new high speed USB device number 2 using fsl-ehci

leds-pca963x 1-0060: setting platform data

android_work: sent uevent USB_STATE=CONNECTED

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

logger: created 256K log 'log_main'

logger: created 256K log 'log_events'

logger: created 256K log 'log_radio'

logger: created 256K log 'log_system'

Cirrus Logic CS42888 ALSA SoC Codec Driver

i2c-core: driver [cs42888] using legacy suspend method

i2c-core: driver [cs42888] using legacy resume method

sgtl5000 0-000a: sgtl5000 revision 17

print_constraints: 0-000a: 850 <--> 1600 mV at 1200 mV normal

hub 2-1:1.0: USB hub found

hub 2-1:1.0: 4 ports detected

android_work: sent uevent USB_STATE=DISCONNECTED

asoc: sgtl5000 <-> imx-ssi.1 mapping ok

Initialize HDMI-audio failed. Load HDMI-video first!

ALSA device list:

  #0: sgtl5000-audio

NET: Registered protocol family 26

TCP cubic registered

NET: Registered protocol family 10

IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

can: controller area network core (rev 20090105 abi 8)

NET: Registered protocol family 29

can: raw protocol (rev 20090105)

can: broadcast manager protocol (rev 20090105 t)

Bluetooth: RFCOMM TTY layer initialized

android_work: sent uevent USB_STATE=CONNECTED

Bluetooth: RFCOMM socket layer initialized

android_work: sent uevent USB_STATE=DISCONNECTED

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

lib80211: common routines for IEEE802.11 drivers

Registering the dns_resolver key type

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

DDR type is DDR3

Bus freq driver module loaded

Bus freq driver Enabled

mxc_dvfs_core_probe

DVFS driver module loaded

regulator_init_complete: VDDD: incomplete constraints, leaving on

rtc-pcf8563 0-0051: low voltage detected, date/time is not reliable.

rtc-pcf8563 0-0051: setting system clock to 2000-08-20 04:31:20 UTC (966745880)

android_work: sent uevent USB_STATE=CONNECTED

mmc1: new high speed SDHC card at address b368

mmcblk0: mmc1:b368 USD   3.72 GiB

mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4

mmcblk0: p4 size 5635614 extends beyond EOD, truncated

android_work: sent uevent USB_STATE=DISCONNECTED

android_work: sent uevent USB_STATE=CONNECTED

android_work: sent uevent USB_STATE=DISCONNECTED

List of all partitions:

1f00              64 mtdblock0  (driver?)

1f02             256 mtdblock2  (driver?)

1f03             768 mtdblock3  (driver?)

1f04             256 mtdblock4  (driver?)

1f05             768 mtdblock5  (driver?)

1f06             256 mtdblock6  (driver?)

1f07            5888 mtdblock7  (driver?)

1f08          253952 mtdblock8  (driver?)

b300         3904512 mmcblk0  driver: mmcblk

  b301           11439 mmcblk0p1 00000000-0000-0000-0000-000000000000

  b302           11439 mmcblk0p2 00000000-0000-0000-0000-000000000000

  b303               1 mmcblk0p3 00000000-0000-0000-0000-000000000000

  b304         2764425 mmcblk0p4 00000000-0000-0000-0000-000000000000

android_work: sent uevent USB_STATE=CONNECTED

  b305          526193 mmcblk0p5 00000000-0000-0000-0000-000000000000

  b306          526193 mmcblk0p6 00000000-0000-0000-0000-000000000000

  b307           11438 mmcblk0p7 00000000-0000-0000-0000-000000000000

  103:00000      11438 mmcblk0p8 00000000-0000-0000-0000-000000000000

No filesystem could mount root, tried:  ext3 ext2 ext4 cramfs squashfs vfat msdos romfs fuseblk

Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(31,0)

[<80050fe4>] (unwind_backtrace+0x0/0x138) from [<8065ceec>] (panic+0x74/0x18c)

[<8065ceec>] (panic+0x74/0x18c) from [<80008db8>] (mount_block_root+0x1e0/0x224)

[<80008db8>] (mount_block_root+0x1e0/0x224) from [<80008fd0>] (mount_root+0xe8/0x108)

[<80008fd0>] (mount_root+0xe8/0x108) from [<80009154>] (prepare_namespace+0x164/0x1c8)

[<80009154>] (prepare_namespace+0x164/0x1c8) from [<80008a10>] (kernel_init+0x108/0x13c)

[<80008a10>] (kernel_init+0x108/0x13c) from [<8004a408>] (kernel_thread_exit+0x0/0x8)

Thanks Jonny

Labels (3)
0 Kudos
Reply
1 Reply

1,438 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jonathan

please look at attached document sect.5.2.1 Booting from NAND on

the i.MX 6DualQuad/6DualLite SABREAI board, how to boot correctly.

IMX6_KK443_200_ANDROID_SOURCE_BSP (REV kk4.4.3_2.0.0)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply