Hi,
Does anyone have a pre-built binary of the libgstmediaplayer.so for IMX6 board?
....../plugins/mediaservice/libgstmediaplayer.so.
Our QT application cannot play (.mp4) videos without this plugin during runtime (even if our app is statically built). We use the QTMultimedia module in our application which uses gstreamer.
If we build the plugin ourselves there are too many arm-version dependencies it needs that is not in our cross compiler environment.
Can anyone help with this?
Regards,
Mark
Hi Mark,
You could take a look at the following thread, also related to libgstmediaplayer.so:
meta-qt5 on master-next does not build video mediaservices
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------