Cannot use mfgtool2-cli on Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot use mfgtool2-cli on Linux

2,531件の閲覧回数
erezamir
Contributor II

Hi,

I am trying to burn uboot and kernel to my QWKS-SCMIMX6 rev2 board.

I am using latest mfgtools downloaded from Quick Start Board for SCM-i.MX 6DQ|NXP 

Observations:

1. I do see the VID/PID of the board with lsusb

2. Tried every legal configuration of SW[2-3] - no influence

3. I've successfully loaded mfg uboot and kernel images with Windows 7 PC and MfgTool2.exe onto the same board and got linux console via serial port (I've got kernel panic at initrc, but thats another story)

The MfgToolLibLog.txt contains the following:

ModuleID[2] LevelID[1]: MxHidDevice::Read() Error reading from device 0x-7 with size 1025.

ModuleID[2] LevelID[1]: Failed to read HAB type from ROM!!!

ModuleID[2] LevelID[1]: Failed to initialize memory!

I suspect something wrong with mfgtoolcli and/or libMfgToolLib.so. Did someone successfully loaded mfg uboot and kernel using those mfgTools and linux host machine?

Additional info: I've already tried Ubuntu 14.04 and 16.04.

Also, I've found source code for mfgtools at GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

A bit of looking into the code reveals that error comes from libusb: LIBUSB_ERROR_TIMEOUT (-7).

Can someone confirm that libMfgToolLib.so works on any Linux setup with QWKS SCM board?

Thanks

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,030件の閲覧回数
tommos23
Contributor III

Has there been any update on this as I am having the same issues with Ubuntu 16.04

0 件の賞賛
返信

2,030件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi, 

Do you mean you are trying to execute mfgtool in a linux host?

It has been tested only on Windows. 

Best Regards,

Alejandro

0 件の賞賛
返信