Cannot play application with -platform eglfs in Yocto 2.4 image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot play application with -platform eglfs in Yocto 2.4 image

1,645件の閲覧回数
wangtsungli
Contributor IV

Hi Community,

I'm using Yocto project imx-4.9.11_1.0.0_ga and I use i.MX6 sabre-SD Quad as my platform.

First to mention, I used Yocto project imx-4.1.15-1.0.0_ga before and build fsl-image-qt5.

For this image, I could run my application with ./application -platform eglfs.

Because I need to use QT version 5.9 so I tried to change it to new Yocto version.

This is the story why I change to imx-4.9.11_1.0.0_ga.

But now I had faced the other problem.

I do the exactly the same thing that I did on imx-4.1.15-1.0.0_ga.

However I the image of fsl-image-qt5-validation-imx and fsl-image-qt5 could not use -platform eglfs.

Below is the condition that I build them.

For fsl-image-qt5-validation-imx, I use this command "bitbake fsl-image-qt5-validation-imx.".

After bitbake is success, I updated my new root file system to my machine.

Everything look perfect, I could see desktop on my panel.

But while I try to run my application with ./application -platform eglfs, it will show there is no command of eglfs.

So I tried to bitbake the other image fsl-image-qt5 and try this one again.

However, it still has no eglfs.

It will show below error message to me.

Available platform plugins are: minimal, offscreen, vnc, wayland-egl, wayland

Question

  1. Why there is no eglfs on new yocto version?
  2. Did I miss anything and cause eglfs is not packing in rootfs?
タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,265件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi tsung

You should stay in 4.1.15, since egl is not supported in L4.9.11, this is for MX8.

Regards

0 件の賞賛
返信

1,265件の閲覧回数
wangtsungli
Contributor IV

Bio_TICFSL 留言:

Hi tsung

 

You should stay in 4.1.15, since egl is not supported in L4.9.11, this is for MX8.

 

Regards

If I need eglfs with qt version 5.8, what should I do?

4.1.15 has eglfs but the qt version is 5.5, it is not high enough for me.

Is there any way that I could build qt 5.8 with 4.1.15 eglfs?

0 件の賞賛
返信