What is the state of pads on i.mx6q during POR and boot procedure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the state of pads on i.mx6q during POR and boot procedure

983件の閲覧回数
cgperson
Contributor II

Hi ,

    I need to have a clear understanding of the pad state during boot procedure to control other chips on my mainboard. I just have a look at IOMUXC_XXX_XXX registers. Dose these registers determine the state? 

    Better to provide the timing diagram to desicrbe the states during boot to let me check my power on configuration strategy  in my design.

ラベル(1)
0 件の賞賛
返信
1 返信

923件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jie

pads state during reset is described in Table 96. 21 x 21 mm Functional Contact

Assignments i.MX6DQ Datasheet

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信