Cannot detect the SD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot detect the SD

1,866件の閲覧回数
eishishibusawa
Contributor III

Dear Sir

Sometimes it does not recognize the SD on the customer board.

Customer uses the i.MX6SX and Linux Version 4.1.15-2.0.

The log is the follows.

sdhci: Tuning procedure failed, falling back to fixed sampling clock
mmc2: tuning execution failed
Waiting for removable media...
mmc2: error -5 whilst initialising SD card


Is there a similar problem?

Best Regards,

Eishi SHIBUSAWA

ラベル(3)
0 件の賞賛
返信
1 返信

1,548件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

one can recheck sd signals layout with sect.3.6.8 High speed signal routing recommendations

i.MX6 System Development User’s Guide :

For SD module interfaces:
– Match data and CMD trace lengths (length delta depends on bus rates)
– CLK should be longer than the longest signal in the Data/CMD group (+5 mils)
— Similar DDR rules must be followed for data, address and control as for SD module interfaces.

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

also for reducing noise one can try to tweak drive strength of sd signals using IOMUXC_SW_PAD_CTL_PAD register

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信