Cannot connect/ succeed to flash with uuu on iMX8QM COM module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot connect/ succeed to flash with uuu on iMX8QM COM module

2,778 Views
dry
Senior Contributor I

I got a module from Kontron based on iMX8QM.

Here is what U-boot shows :

U-Boot 2019.04-4.19.35-1.1.0+g4d37753 (Jun 02 2022 - 21:24:12 +0000)

CPU: NXP i.MX8QM RevB A53 at 1200 MHz at 33C

BuildInfo:
- SCFW 4e91f37b, SECO-FW d7523fe8, IMX-MKIMAGE 1c2277b9, ATF 70fa7bc
- U-Boot 2019.04-4.19.35-1.1.0+g4d37753

 

I'm trying to burn in / update Linux image - or actually at the moment any image, U-boot or /and Linux  - using the UUU utility, with no success.

I can set to board/COM into the manufacturing mode per board doc, where supposedly it should be ready to use for UUU. 

This is what the dev shows up as when I plug it into Win10 PC when the module is in "recovery" or manufacturing mode:

dry_0-1662511956875.png

 

uuu -lsusb
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.243-0-ged48c51

Connected Known USB Devices
        Path     Chip    Pro     Vid     Pid     BcdVersion
        ==================================================
        1:83114  MX8QM   SDPS:   0x1FC9 0x0129   0x0002

 

And from here I cannot get anywhere ...  E.g:

>uuu -b emmc  kontron-image-qt5-validation-samx-kontron-samx8-qm.sdcard.bz2/*
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.243-0-ged48c51

Success 0    Failure 1


1:83114  1/ 1 [HID(W):LIBUSB_ERROR_PIPE              ] SDPS: boot -f kontron-image-qt5-validation-samx-kontron-samx8-qm.

 

uuu -b emmc imx-boot-kontron-samx8-qm-fspi-8GB.bin
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.243-0-ged48c51

Success 0    Failure 1


1:83114  1/ 1 [HID(W):LIBUSB_ERROR_PIPE              ] SDPS: boot -f imx-boot-kontron-samx8-qm-fspi-8GB.bin

 

There is just a delay, then device resets and back into the default internally programmed u-boot shell.

Always ends up in that.

There is very little helpful messages from uuu.  Is the device correct, why does it always end into libusb error ... ?  

 

 

0 Kudos
Reply
4 Replies

2,718 Views
dry
Senior Contributor I

@jimmychan 

Please assist with the following issue I'm having.

Firstly, I can flash flash_scfw.bin - that is, my own built image of the scfw from the official sources, it is flashed and started Ok as I can very by seing SCFW traces on a UART (built with debug enabled).

 

 

dry_1-1664407363632.png

But anything seems large in size - like image with U-boot - FAILS to be uploaded & started, at least per the UUU traces. 
In my test I try to upload the "flash" image (without linux) with U-boot as was created by Yocto imx8qm (my soc) build. In this case I get same error trace from UUU as I have originally posted, and the board re-starts:

dry_2-1664407648755.png

So why ... ? Is this a USB transfer problem or ..?

I'm attaching the firmware blob - this was generated by Yocto , under ... imx-boot/0.2-r0/git/iMX8QM/, file flash.bin

 

0 Kudos
Reply

2,769 Views
dry
Senior Contributor I

If I start the "fastboot" from inside the U-boot, then I can update U-boot, rootfs using the FB protocol.

But need to figure out how I can do update over SPD(s?) too, in case U-boot is kaputt.

0 Kudos
Reply

2,749 Views
jimmychan
NXP TechSupport
NXP TechSupport

Please read the UUU.pdf  for how to write the script to program the board.

0 Kudos
Reply

2,743 Views
dry
Senior Contributor I

Yea, when I will need to write one I shall.

 

Could you also please improve the English version documentation of UUU .. ? 

Some of the messages and the text in the doc look like uses English letters but not making much sense.

0 Kudos
Reply