Can we use SDIO interface [not USB]Wifi Card for Android ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can we use SDIO interface [not USB]Wifi Card for Android ?

4,353 次查看
ThanarajS
Contributor III

Hi All,

   We have SDIO Interface supported wifi card, Can we use that module for android driver porting ?

   We tried but wifi card is not detecting in Android Kernel.

   Please help me to use SDIO Interface based Wi-Fi Card.

Regards,

Thanaraj.

Regards,
Thanaraj Subramani
标签 (5)
0 项奖励
回复
2 回复数

3,547 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Thanaraj

yes it can be used, please refer to attached Linux Manual

Chapter 46 Wi-Fi BCM4339 Driver, the same is for Android as

described in Release Notes Table 2. Features. Usually porting

guidelines are provided by chip vendor.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,547 次查看
ThanarajS
Contributor III

Hi igor,

   We are not using BCM Driver. But Generally if we insert the SDIO Card it should get detected by kernel. But here SDIO Card is detected and immediately card removed.

================================================================================================

LOG:

================================================================================================

8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
dhd_module_init in
Power-up adapter 'DHD generic adapter'
wifi_platform_bus_enumerate device present 1
mmc1: new high speed SDIO card at address fffd
failed to power up DHD generic adapter, 3 retry left
wifi_platform_bus_enumerate device present 0
mmc1: card fffd removed
wifi_platform_bus_enumerate device present 1
mmc1: new high speed SDIO card at address fffd
failed to power up DHD generic adapter, 2 retry left
wifi_platform_bus_enumerate device present 0
mmc1: card fffd removed
wifi_platform_bus_enumerate device present 1
mmc1: new high speed SDIO card at address fffd
failed to power up DHD generic adapter, 1 retry left
wifi_platform_bus_enumerate device present 0
mmc1: card fffd removed
wifi_platform_bus_enumerate device present 1
mmc1: new high speed SDIO card at address fffd
failed to power up DHD generic adapter, 0 retry left
wifi_platform_bus_enumerate device present 0
mmc1: card fffd removed
failed to power up DHD generic adapter, max retry reached**
input: gpio-keys as /devices/soc0/gpio-keys/input/input12

=========================================================================================================

Anything we need to enable from host controller side or in kernel menuconfig ?

Please suggest idea to fix this..

Thanks,

Thanaraj.

Regards,
Thanaraj Subramani
0 项奖励
回复