Hi,
We have a requirement where, We want to play two video of resolution 1080p @ 30fps (worst case 1080p @ 24fps) on two different video ports (which are connected to two different LCDs) simultaneously.
So, My first question would be, Is this possible to playback 2 videos of 1080p simultaneously on two different port?
If that is possible then, Which of the below option is feasible or supported?
1) Using two RGB ports.
2) Using 1 RGB and 1 dual LVDS port.
Video type of 1080p @ 30fps is h264 for which we want to perform above operation.
Thanks,
Pratik
Hello,
Please refer to the following Dual 1080p video playback in sabresd-imx6d
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------