Can't see spi to /dev/spidev imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't see spi to /dev/spidev imx6

2,086 Views
maxime_metayer
Contributor I
Hello everybody,  I run the debian linux distribution provided by the compulab site for the cl-som-imx6ul
but I do not see the dev / spidev interface.  can you help me please?
Labels (2)
Tags (3)
0 Kudos
Reply
2 Replies

1,775 Views
igorpadykov
NXP Employee
NXP Employee

Hi Romain

for spidev one can look at below links and post issue on compulab forum

VAR-SOM-MX6 SPI - Variscite Wiki 

CM-FX6: Linux: Kernel - Compulab Mediawiki 

How to interface MCU with i.MX6 over SPI interface? - Toradex Community 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,775 Views
maxime_metayer
Contributor I

Hi Igor,

Thank's for you answer, but I use a Cl-SOM-IMX6UL card. Do you think these changes are applicable  to this type of card ? 

Best regards,

Romain

0 Kudos
Reply