Can't see spi to /dev/spidev imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't see spi to /dev/spidev imx6

2,135件の閲覧回数
maxime_metayer
Contributor I
Hello everybody,  I run the debian linux distribution provided by the compulab site for the cl-som-imx6ul
but I do not see the dev / spidev interface.  can you help me please?
ラベル(2)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,824件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Romain

for spidev one can look at below links and post issue on compulab forum

VAR-SOM-MX6 SPI - Variscite Wiki 

CM-FX6: Linux: Kernel - Compulab Mediawiki 

How to interface MCU with i.MX6 over SPI interface? - Toradex Community 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,824件の閲覧回数
maxime_metayer
Contributor I

Hi Igor,

Thank's for you answer, but I use a Cl-SOM-IMX6UL card. Do you think these changes are applicable  to this type of card ? 

Best regards,

Romain

0 件の賞賛
返信