Can't see spi to /dev/spidev imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't see spi to /dev/spidev imx6

2,056 次查看
maxime_metayer
Contributor I
Hello everybody,  I run the debian linux distribution provided by the compulab site for the cl-som-imx6ul
but I do not see the dev / spidev interface.  can you help me please?
标签 (2)
标记 (3)
0 项奖励
回复
2 回复数

1,745 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Romain

for spidev one can look at below links and post issue on compulab forum

VAR-SOM-MX6 SPI - Variscite Wiki 

CM-FX6: Linux: Kernel - Compulab Mediawiki 

How to interface MCU with i.MX6 over SPI interface? - Toradex Community 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,745 次查看
maxime_metayer
Contributor I

Hi Igor,

Thank's for you answer, but I use a Cl-SOM-IMX6UL card. Do you think these changes are applicable  to this type of card ? 

Best regards,

Romain

0 项奖励
回复