I am working on the imx8m mini with imx334 camera sensor so my issues is that sensor is registered and v4l2 also registered but i am not able get the /dev/v4l2-subdev. media-ctl -p command is also not working it is showing error Failed to enumerate /dev/media0 (-2)
my biggest questions is how to add ISP on my imx8m-mini?
here is my driver info it is not even capturing the image.
my linux kernel version is 5.15.48+gb6597629c15c
Driver Info:
Driver name : mx6s-csi
Card type : i.MX6S_CSI
Bus info : platform:32e20000.csi1_bridge
Driver version : 5.10.52
Capabilities : 0x84200001
Video Capture
Streaming
Extended Pix Format
Device Capabilities
Device Caps : 0x04200001
Video Capture
Streaming
Extended Pix Format
Priority: 0
Video input : 0 (Camera: ok)
Format Video Capture:
Width/Height : 0/0
Pixel Format : ''
Field : Any
Bytes per Line : 0
Size Image : 0
Colorspace : Default
Transfer Function : Default (maps to Rec. 709)
YCbCr/HSV Encoding: Default (maps to ITU-R 601)
Quantization : Default (maps to Full Range)
Flags :
Crop Capability Video Capture:
Bounds : Left 0, Top 0, Width 0, Height 0
Default : Left 0, Top 0, Width 0, Height 0
Pixel Aspect: 1/1
Selection Video Capture: crop, Left 0, Top 0, Width 0, Height 0, Flags:
Selection Video Capture: crop_default, Left 0, Top 0, Width 0, Height 0, Flags:
Selection Video Capture: crop_bounds, Left 0, Top 0, Width 0, Height 0, Flags:
Selection Video Capture: compose, Left 0, Top 0, Width 0, Height 0, Flags:
Selection Video Capture: compose_default, Left 0, Top 0, Width 0, Height 0, Flags:
Selection Video Capture: compose_bounds, Left 0, Top 0, Width 0, Height 0, Flags:
Selection Video Capture: compose_padded, Left 0, Top 0, Width 0, Height 0, Flags:
Selection Video Capture: native_size, Left 0, Top 0, Width 0, Height 0, Flags: