Hello
My board is imx6q-sdb.
I have a question about how to make an uImage for MfgTool.
Before MfgTool burn image to flash, CPU will boot up first.
The MfgTool use two uImages,one for bootint up, another using to burn flash.
Now,I use the uImage which be compiled by myself.
When the MfgTool make the CPU boot up,it can not mount file system.
When I use the origin uImage include by MfgTool,CPU will start UTP when it finish initializing kernel.
Q:
What is UTP?
What do I need to modify my linux kernel?
UART print the blow information.
Using origin uImage:
......
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
Bus freq driver module loaded
Bus freq driver Enabled
mxc_dvfs_core_probe
DVFS driver module loaded
regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on
regulator_init_complete: SPKVDD: incomplete constraints, leaving on
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)
Freeing init memory: 200K
Starting UTP
ln: /etc/mtab: File exists
disable turn off display
Starting the hotplug events dispatcher udevd
udevd (2001): /proc/2001/oom_adj is deprecated, please use /proc/2001/oom_score_
adj instead.
Using my uImage:
......
DVFS driver module loaded
regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)
List of all partitions:
1f00 1024 mtdblock0 (driver?)
1f01 31744 mtdblock1 (driver?)
b300 7757824 mmcblk0 driver: mmcblk
b301 7747584 mmcblk0p1 00000000-0000-0000-0000-000000000000
b310 2048 mmcblk0boot1 (driver?)
b308 2048 mmcblk0boot0 (driver?)
No filesystem could mount root, tried: jffs2
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
[<80044854>] (unwind_backtrace+0x0/0xf8) from [<805067d4>] (panic+0x74/0x18c)